Test it with: uuu.exe -b emmc_all .\imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot .\imx-image-full-imx93evk.wic
Image downloaded from Embedded Linux for i.MX Applications Processors | NXP Semiconductors
Test board: i.MX93-evk for 11x11
Regards
Harvey
Hi,
Please refer to the document UUU.pdf with uuu tool for how to flash emmc
ex: uuu -b emmc <bootloader>
uuu -b emmc_all <bootloader> <rootfs.wic.zst/*>
You can also refer to <4 Booting Linux OS> of <IMX_LINUX_USERS_GUIDE.pdf>
Regards
Harvey
Hi @Harvey021
I have tried this but getting a error as :
./uuu -b emmc_all u-boot.bin imx-image-full-imx93-11x11-lpddr4x-evk-20240829072649.rootfs.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
Success 0 Failure 1
3:4-DAAE92E6 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f u-boot.bin -scanlimited 0x800000
Also please confirm the bootloader binary I tried to flash these 3 bootloader binaries but reporting same error please help.
Imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot
u-boot.bin
u-boot-imx93-11x11-lpddr4x-evk.bin
I have tried this too but same error I am getting what could be the possible reason?
./uuu -b emmc imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
Success 0 Failure 1
3:4-DAAE92E6 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot
and
./uuu -b emmc_all imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot imx-image-full-imx93-11x11-lpddr4x-evk-20240829072649.rootfs.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
Success 0 Failure 0
Success 0 Failure 1
3:4-DAAE92E6 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot -sca
Test it with: uuu.exe -b emmc_all .\imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot .\imx-image-full-imx93evk.wic
Image downloaded from Embedded Linux for i.MX Applications Processors | NXP Semiconductors
Test board: i.MX93-evk for 11x11
Regards
Harvey
Hi @harvey
Actually uuu -lsusb is detecting the board but could not flash
only this error I am getting :
3:1-3661BD70 1/ 1 [HID(W): LIBUSB_ERROR_TIMEOUT (-7) ] SDPS: boot -scanterm -f imx-boot-imx91-11x11-lpddr4-evk-sd.bin-flash_singleboot -scan
Hi,
Have a test on host-Ubuntu 20.04-as below for your reference.
Image downloaded from the link https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX93&appType=license
Cli: sudo uuu -b emmc_all imx-boot-imx93evk-sd.bin-flash_singleboot imx-image-full-imx93evk.wic
or sudo uuu -b emmc_all imx-image-full-imx93evk.wic
Both way work on my side.
Regards
Harvey
Hi,
I am also using ubuntu 20.04 but still the issue is same as I tried to flash the image which you suggested.
My uuu version is: uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
is there any specific uuu version that we need to use?
Should not related to uuu version.
However, the one I tested is
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.11-0-g7c0fb61
By the way, what part number is your board?
Regards
Harvey
Would suggest to check your Ubuntu settings and my host is not virtual machine
To avoid the image to be flashed with some corruption, like that copy from Windows by tools. better download it from Linux platform.
Regards
Harvey