MIPI CSI port from Cortex-M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI port from Cortex-M4

1,899 Views
zsv82
Contributor I

Hello! Is it possible to use MIPI CSI port in IMX8M-mini SoM from Cortex-M4 co-processor? Thank you

0 Kudos
Reply
2 Replies

1,754 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sam,

Is not possible to use the MIPI-CSI with cortex M4 but one can look at sect.2.8 Remote Processor Messaging Linux Manual

in Linux L4.14.98_2.0.0 Documentation

Where you shares msg between two cores.

Regards

0 Kudos
Reply

1,754 Views
zsv82
Contributor I

Thank you...But i would like to start frame capture immediately after powering-on without waiting for Linux-booting. Probably i have to use another (bare-metal) microcontroller for this tasks 

0 Kudos
Reply