MIPI_CSI Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI_CSI Error

1,731件の閲覧回数
santhosh2
Contributor IV

Hi,

I have connected the Camera to MIPI_CSI and when i run the gstreamer command I'm getting the below error

root@iWave-G27M:~#export DISPLAY=:0
root@iWave-G27M:~# gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw ! videoconvert ! ximagesink
Setting pipeline to PAUSED ...
Pipeline [i s2 5l6i2v.e5 3a7n7d9 7do]e sm xnco_tis nie.e0d:  PCRaEnR'OtL Lf i.n.d. s
Suebtdteivng
 pipeline to PLAYING ...
New clock: GstSystemClock
[ 2562.550871] mxc_isi.0: Can't find subdev
[ 2562.555044] mxc_isi.0: Can't find subdev
[ 2562.559245] mxc_isi.0: Can't find subdev
[ 2562.563423] mxc_isi.0: Can't find subdev
[ 2562.567575] mxc_isi.0: Can't find subdev
[ 2562.571731] mxc_isi.0: Can't find subdev
[ 2562.575859] mxc_isi.0: Can't find subdev
[ 2562.581833] (null): mxc_isi_source_fmt_init, No remote pad found!
[ 2562.587971] bypass csc
[ 2562.590340] input fmt RG10
[ 2562.593079] output fmt YUYV
[ 2562.595910] mxc-isi 58100000.isi: input_size(0,0), output_size(200,320)
[ 2562.602575] mxc_isi.0: Can't find subdev
^Chandling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:00:03.765367869
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Freeing pipeline ...
root@iWave-G27M:~#

Let me know how can i resolve

Regards

0 件の賞賛
返信
1 返信

1,528件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

seems you are using third party board which is supported by its vendor,

issue may be posted on its support forum

https://www.iwavesystems.com/imx8-quadmax-smarc-som.html 

alternatively one can try with nxp reference boards and software:

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信