MIPI CSI-2 skip first data lane

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIPI CSI-2 skip first data lane

1,844 次查看
adc1
Contributor IV

Hi,
I'm trying to use a ov5640 camera configuring just a single lane data, in particular I'm trying to use just the second one. Is it possible? Can I exclude first lane?

Referring to this post Single Lane Mipi interface to i.mx6 , I'm using "One lane mode" and setup register 0x4800 MIPI CTRL 00  Bit[3] to 1 (0 Use lane1 as default data lane, 1 Use lane2 as default data lane).

Using a ov13850, I have also tried to use only two-lanes but data is correctly transferred only if I use first two ones, if I enable lanes 3 and 4 I obtain a MIPI data transfer error. So, is it possible to exclude first lanes?


thank you, regards
Andrea

标签 (3)
标记 (3)
0 项奖励
回复
1 回复

1,527 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I am afraid this is impossible to use only lanes 2 and 3 of i.MX6 MIPI CSI.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------