MIPI CSI-2 capabilities vs data lanes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI CSI-2 capabilities vs data lanes

ソリューションへジャンプ
2,584件の閲覧回数
g_moreno
Contributor III

Hello,

About the MIPI CSI-2 capabilities, I would like to confirm if the following calculation is correct: for 1920 x 1080 @ 30 fps in video mode, do I need at least 3 data lanes?

F = 1920 * 1080 * 30 * 1.35 * 2 (cycles per pixel) = 168MHz

According to i.MX6QRM Rev. 2 page 2733, maximum bandwith for 2 lanes is 125MHz.

Thank you!

ラベル(2)
0 件の賞賛
返信
1 解決策
2,387件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guillermo

I believe your calculations are correct, 3 data lanes are needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,388件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Guillermo

I believe your calculations are correct, 3 data lanes are needed.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,387件の閲覧回数
g_moreno
Contributor III

Thank you Igor.

0 件の賞賛
返信