MIMXRT1176 power and DCDC module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1176 power and DCDC module

ソリューションへジャンプ
1,920件の閲覧回数
muxeu
Contributor II

Hello.

Please tell me:

  1. How do the PMIC_STBY_REQ and PMIC_ON_REQ signals work?
  2. Do I understand correctly that the output voltage of the DCDC module is adjusted in the CTRL1 register?
  3. How do the GPIO_SNVS_xx signals work?
タグ(2)
0 件の賞賛
返信
1 解決策
1,901件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @muxeu,

  1. How do the PMIC_STBY_REQ and PMIC_ON_REQ signals work?

In the chapter 25.3.2 explains in more detail the behavior of this signals.

 

SNVS_PMIC_STBY_REQ outputs a high-level signal under Suspend Mode (Stop Mode).

After it entry into SNVS mode, it will drive PMIC_ON_REQ to low, and resume to high on waking up, this can be used to control power supply for SOC.

 

  1. Do I understand correctly that the output voltage of the DCDC module is adjusted in the CTRL1 register?

 

That's right, depending of the mode (standby/buck) is the register to use.

 

  1. How do the GPIO_SNVS_xx signals work?

 

The signal has two functionalities, the GPIO and the tamper, which one do you mean?

 

Best Regards,
Alexis Andalon

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,902件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @muxeu,

  1. How do the PMIC_STBY_REQ and PMIC_ON_REQ signals work?

In the chapter 25.3.2 explains in more detail the behavior of this signals.

 

SNVS_PMIC_STBY_REQ outputs a high-level signal under Suspend Mode (Stop Mode).

After it entry into SNVS mode, it will drive PMIC_ON_REQ to low, and resume to high on waking up, this can be used to control power supply for SOC.

 

  1. Do I understand correctly that the output voltage of the DCDC module is adjusted in the CTRL1 register?

 

That's right, depending of the mode (standby/buck) is the register to use.

 

  1. How do the GPIO_SNVS_xx signals work?

 

The signal has two functionalities, the GPIO and the tamper, which one do you mean?

 

Best Regards,
Alexis Andalon

0 件の賞賛
返信
1,891件の閲覧回数
muxeu
Contributor II

Thanks for answers. Interested in the operation of the GPIO_SNVS signals in relation to the SNVS module.

0 件の賞賛
返信
1,885件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @muxeu,

The SNVS mention is due to the tamper feature related to this pins. In the MIMXRT1176 is not present this feature so it will only work as GPIO.

Best Regards,
Alexis Andalon

0 件の賞賛
返信