MIMXRT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMXRT1064

1,270 次查看
StarMao159376
Contributor II

Does mimxrt1064 support local bus?

0 项奖励
回复
1 回复

1,263 次查看
Yuri
NXP Employee
NXP Employee

@StarMao159376 
Hello,

   If I understand the question correctly, the i.MX RT does not support a local bus
(internal bus, common for all i.MX RT internal modules)  for external devices. 
  The most close for customer's purposes - I think - is the SEMC (Smart External Memory
Controller).
     "The SEMC is a multi-standard memory controller optimized for both high-performance
and low pin-count. It can support multiple external memories in the same
application with shared address and data pins. The interface supported includes SDRAM,
NOR Flash, SRAM, and NAND Flash, as well as 8080 display interface."

Regards,
Yuri.

0 项奖励
回复