MIMXRT1064 INTERNAL FLASH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1064 INTERNAL FLASH

Jump to solution
3,553 Views
sandeepc
Contributor IV

hi i want store some kmph data to the internal flash of the mimxrt1064 i gone through the nxp community i got to know that we can use evkmimxrt1064_flexspi_nor_polling_transfer example to understand so while going through that 

link 1: 

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-the-RT1064-on-chip-flash-as-NVM/ta-p/...

==> the example is used flexspi1 i.e external flash so internal flash is connected flexspi2

==> the ROM bootloader will configure the pins of this FlexSPI interface  So flexspi configuration is it required or not

 

nxp.png

 

                   ==> where can i get Flash size and example sector means

==> i didnt get what is meant by  customLUT? and also i didnt get meaning of these two lines

  1. Erase sector command of the on-chip flash is 0x20 instead of 0xD7. 
  2. Exchange the FLEXSPI command index for NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD and NOR_CMD_LUT_SEQ_IDX_READ_NORMAL to align with XIP settings.

i gone at the last provided link i didnt get api reference manal to understan what it is actually api mean and its argumentsf ew api iam mentionning 

1) status = flexspi_nor_get_vendor_id(EXAMPLE_FLEXSPI, &vendorID);

2)  status = flexspi_nor_enable_quad_mode(EXAMPLE_FLEXSPI);

3) status = flexspi_nor_flash_erase_sector(EXAMPLE_FLEXSPI, EXAMPLE_SECTOR * SECTOR_SIZE);

4)  status =
flexspi_nor_flash_page_program(EXAMPLE_FLEXSPI, EXAMPLE_SECTOR * SECTOR_SIZE, (void *)s_nor_program_buffer);

few more are there where can i found this api maual 

and in which section will be helpfull understand well i.MX RT1064 Processor Reference
Manual
Document Number: IMXRT1064RM
Rev. 2,

@kerryzhou @IMXRT1050 

0 Kudos
Reply
1 Solution
3,520 Views
sandeepc
Contributor IV

hi community update to my my quetion i had done modification by referring below links i compiled and its working but i didnt find ANY API TO READ THE DATA FROM FLASH if i get that api i can verify the data which have writeen 

1) iam sharing my code below if any correction required please let me 

2)where can i found the api reference manual for above mentioned functions

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-the-RT1064-on-chip-flash-as-NVM/ta-p/...

https://community.nxp.com/t5/i-MX-RT/RT1050-QSPI-flash-change-to-Winbond-W25Q32JV-3-3V/m-p/904534

https://community.nxp.com/t5/MCUXpresso-General/I-can-not-erase-QSPI-Flash-W25Q32JV/m-p/884895

after modification my code is below iam attaching my project please go through it and also iam attaching my file 

 

/*
 * Copyright (c) 2016, Freescale Semiconductor, Inc.
 * Copyright 2016-2018 NXP
 * All rights reserved.
 *
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */
 
#include "fsl_flexspi.h"
#include "app.h"
#include "fsl_debug_console.h"
#include "fsl_cache.h"
 
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_common.h"
/*******************************************************************************
 * Definitions
 ******************************************************************************/
/*******************************************************************************
 * Prototypes
 ******************************************************************************/
 
/*******************************************************************************
 * Variables
 ******************************************************************************/
/* Program data buffer should be 4-bytes alignment, which can avoid busfault due to this memory region is configured as
   Device Memory by MPU. */
SDK_ALIGN(static uint8_t s_nor_program_buffer[256], 4);
static uint8_t s_nor_read_buffer[256];
 
extern status_t flexspi_nor_flash_erase_sector(FLEXSPI_Type *base, uint32_t address);
extern status_t flexspi_nor_flash_page_program(FLEXSPI_Type *base, uint32_t dstAddr, const uint32_t *src);
extern status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId);
extern status_t flexspi_nor_enable_quad_mode(FLEXSPI_Type *base);
extern status_t flexspi_nor_erase_chip(FLEXSPI_Type *base);
extern void flexspi_nor_flash_init(FLEXSPI_Type *base);
/*******************************************************************************
 * Code
 ******************************************************************************/
flexspi_device_config_t deviceconfig = {
.flexspiRootClk       = 120000000,
.flashSize            = FLASH_SIZE,
.CSIntervalUnit       = kFLEXSPI_CsIntervalUnit1SckCycle,
.CSInterval           = 2,
.CSHoldTime           = 3,
.CSSetupTime          = 3,
.dataValidTime        = 0,
.columnspace          = 0,
.enableWordAddress    = 0,
.AWRSeqIndex          = 0,
.AWRSeqNumber         = 0,
.ARDSeqIndex          = NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD,
.ARDSeqNumber         = 1,
.AHBWriteWaitUnit     = kFLEXSPI_AhbWriteWaitUnit2AhbCycle,
.AHBWriteWaitInterval = 0,
};
 
const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {
/* Normal read mode -SDR */
[4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x03, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL + 1] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Fast read mode - SDR */
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x0B, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST + 1] = FLEXSPI_LUT_SEQ(
kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x08, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Fast read quad mode - SDR */
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x6B, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD + 1] = FLEXSPI_LUT_SEQ(
kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x08, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04),
 
/* Read extend parameters */
[4 * NOR_CMD_LUT_SEQ_IDX_READSTATUS] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x81, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Write Enable */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Erase Sector  */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x20, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
 
/* Page Program - single mode */
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x02, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE + 1] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Page Program - quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x32, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD + 1] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_4PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Read ID */
[4 * NOR_CMD_LUT_SEQ_IDX_READID] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9F, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Enable Quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Enter QPI mode */
[4 * NOR_CMD_LUT_SEQ_IDX_ENTERQPI] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x35, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Exit QPI mode */
[4 * NOR_CMD_LUT_SEQ_IDX_EXITQPI] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0xF5, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Read status register */
[4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x05, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Erase whole chip */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASECHIP] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xC7, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
};
 
 
int main(void)
{
uint32_t i = 0;
status_t status;
uint8_t vendorID = 0;
 
BOARD_ConfigMPU();
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitDebugConsole();
 
flexspi_nor_flash_init(EXAMPLE_FLEXSPI);
 
PRINTF("\r\nFLEXSPI example started!\r\n");
 
/* Get vendor ID. */
status = flexspi_nor_get_vendor_id(EXAMPLE_FLEXSPI, &vendorID);
if (status != kStatus_Success)
{
return status;
}
PRINTF("Vendor ID: 0x%x\r\n", vendorID);
 
#if !(defined(XIP_EXTERNAL_FLASH))
/* Erase whole chip . */
PRINTF("Erasing whole chip over FlexSPI...\r\n");
 
status = flexspi_nor_erase_chip(EXAMPLE_FLEXSPI);
if (status != kStatus_Success)
{
return status;
}
PRINTF("Erase finished !\r\n");
 
#endif
 
/* Enter quad mode. */
status = flexspi_nor_enable_quad_mode(EXAMPLE_FLEXSPI);
if (status != kStatus_Success)
{
return status;
}
 
/* Erase sectors. */
PRINTF("Erasing Serial NOR over FlexSPI...\r\n");
status = flexspi_nor_flash_erase_sector(EXAMPLE_FLEXSPI, EXAMPLE_SECTOR * SECTOR_SIZE);
if (status != kStatus_Success)
{
PRINTF("Erase sector failure !\r\n");
return -1;
}
 
memset(s_nor_program_buffer, 0xFFU, sizeof(s_nor_program_buffer));
 
DCACHE_InvalidateByRange(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE, FLASH_PAGE_SIZE);
 
memcpy(s_nor_read_buffer, (void *)(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE),
sizeof(s_nor_read_buffer));
 
if (memcmp(s_nor_program_buffer, s_nor_read_buffer, sizeof(s_nor_program_buffer)))
{
PRINTF("Erase data -  read out data value incorrect !\r\n ");
return -1;
}
else
{
PRINTF("Erase data - successfully. \r\n");
}
 
for (i = 0; i < 0xFFU; i++)
{
s_nor_program_buffer[i] = i;
}
 
status =
flexspi_nor_flash_page_program(EXAMPLE_FLEXSPI, EXAMPLE_SECTOR * SECTOR_SIZE, (void *)s_nor_program_buffer);
if (status != kStatus_Success)
{
PRINTF("Page program failure !\r\n");
return -1;
}
 
DCACHE_InvalidateByRange(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE, FLASH_PAGE_SIZE);
 
memcpy(s_nor_read_buffer, (void *)(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE),
sizeof(s_nor_read_buffer));
 
if (memcmp(s_nor_read_buffer, s_nor_program_buffer, sizeof(s_nor_program_buffer)) != 0)
{
PRINTF("Program data -  read out data value incorrect !\r\n ");
return -1;
}
else
{
PRINTF("Program data - successfully. \r\n");
}
 
while (1)
{
}
}

 

status_t flexspi_nor_enable_quad_mode(FLEXSPI_Type *base)
{
flexspi_transfer_t flashXfer;
status_t status;
uint32_t writeValue =0x0200;// FLASH_QUAD_ENABLE;

#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
flexspi_cache_status_t cacheStatus;
flexspi_nor_disable_cache(&cacheStatus);
#endif

/* Write enable */
status = flexspi_nor_write_enable(base, 0);

if (status != kStatus_Success)
{
return status;
}

/* Enable quad mode. */
flashXfer.deviceAddress = 0;
flashXfer.port = FLASH_PORT;
flashXfer.cmdType = kFLEXSPI_Write;
flashXfer.SeqNumber = 1;
flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG;
flashXfer.data = &writeValue;
// flashXfer.dataSize = 1;
flashXfer.dataSize = 2;


status = FLEXSPI_TransferBlocking(base, &flashXfer);
if (status != kStatus_Success)
{
return status;
}

status = flexspi_nor_wait_bus_busy(base);

/* Do software reset. */
FLEXSPI_SoftwareReset(base);

#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
flexspi_nor_enable_cache(cacheStatus);
#endif

return status;
}

@kerryzhou @michael_imxrt @IMXRT1050 

 

View solution in original post

0 Kudos
Reply
3 Replies
3,512 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sandeepc ,

  You make things complicate, and refer to the wrong code for the internal flash.

  Please refer to this code:

SDK_2_13_0_EVK-MIMXRT1064\boards\evkmimxrt1064\driver_examples\flexspi\nor_internal\polling_transfer

  You can operate the internal flash directly, the internal flash is the winbond flash.

  Please try it again.

  If you can't find this project, please download the new SDK:

https://mcuxpresso.nxp.com/

 

Wish it helps you!

Best Regards,

kerry

0 Kudos
Reply
3,500 Views
sandeepc
Contributor IV
thaank you kerryzhou it is working fine now both example and as well as below replied code
3,521 Views
sandeepc
Contributor IV

hi community update to my my quetion i had done modification by referring below links i compiled and its working but i didnt find ANY API TO READ THE DATA FROM FLASH if i get that api i can verify the data which have writeen 

1) iam sharing my code below if any correction required please let me 

2)where can i found the api reference manual for above mentioned functions

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-use-the-RT1064-on-chip-flash-as-NVM/ta-p/...

https://community.nxp.com/t5/i-MX-RT/RT1050-QSPI-flash-change-to-Winbond-W25Q32JV-3-3V/m-p/904534

https://community.nxp.com/t5/MCUXpresso-General/I-can-not-erase-QSPI-Flash-W25Q32JV/m-p/884895

after modification my code is below iam attaching my project please go through it and also iam attaching my file 

 

/*
 * Copyright (c) 2016, Freescale Semiconductor, Inc.
 * Copyright 2016-2018 NXP
 * All rights reserved.
 *
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */
 
#include "fsl_flexspi.h"
#include "app.h"
#include "fsl_debug_console.h"
#include "fsl_cache.h"
 
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_common.h"
/*******************************************************************************
 * Definitions
 ******************************************************************************/
/*******************************************************************************
 * Prototypes
 ******************************************************************************/
 
/*******************************************************************************
 * Variables
 ******************************************************************************/
/* Program data buffer should be 4-bytes alignment, which can avoid busfault due to this memory region is configured as
   Device Memory by MPU. */
SDK_ALIGN(static uint8_t s_nor_program_buffer[256], 4);
static uint8_t s_nor_read_buffer[256];
 
extern status_t flexspi_nor_flash_erase_sector(FLEXSPI_Type *base, uint32_t address);
extern status_t flexspi_nor_flash_page_program(FLEXSPI_Type *base, uint32_t dstAddr, const uint32_t *src);
extern status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *base, uint8_t *vendorId);
extern status_t flexspi_nor_enable_quad_mode(FLEXSPI_Type *base);
extern status_t flexspi_nor_erase_chip(FLEXSPI_Type *base);
extern void flexspi_nor_flash_init(FLEXSPI_Type *base);
/*******************************************************************************
 * Code
 ******************************************************************************/
flexspi_device_config_t deviceconfig = {
.flexspiRootClk       = 120000000,
.flashSize            = FLASH_SIZE,
.CSIntervalUnit       = kFLEXSPI_CsIntervalUnit1SckCycle,
.CSInterval           = 2,
.CSHoldTime           = 3,
.CSSetupTime          = 3,
.dataValidTime        = 0,
.columnspace          = 0,
.enableWordAddress    = 0,
.AWRSeqIndex          = 0,
.AWRSeqNumber         = 0,
.ARDSeqIndex          = NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD,
.ARDSeqNumber         = 1,
.AHBWriteWaitUnit     = kFLEXSPI_AhbWriteWaitUnit2AhbCycle,
.AHBWriteWaitInterval = 0,
};
 
const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {
/* Normal read mode -SDR */
[4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x03, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL + 1] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Fast read mode - SDR */
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x0B, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST + 1] = FLEXSPI_LUT_SEQ(
kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x08, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Fast read quad mode - SDR */
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x6B, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD + 1] = FLEXSPI_LUT_SEQ(
kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x08, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04),
 
/* Read extend parameters */
[4 * NOR_CMD_LUT_SEQ_IDX_READSTATUS] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x81, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Write Enable */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Erase Sector  */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x20, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
 
/* Page Program - single mode */
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x02, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE + 1] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Page Program - quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x32, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
[4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD + 1] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_4PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Read ID */
[4 * NOR_CMD_LUT_SEQ_IDX_READID] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9F, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Enable Quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Enter QPI mode */
[4 * NOR_CMD_LUT_SEQ_IDX_ENTERQPI] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x35, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Exit QPI mode */
[4 * NOR_CMD_LUT_SEQ_IDX_EXITQPI] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0xF5, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
 
/* Read status register */
[4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x05, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),
 
/* Erase whole chip */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASECHIP] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xC7, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0),
};
 
 
int main(void)
{
uint32_t i = 0;
status_t status;
uint8_t vendorID = 0;
 
BOARD_ConfigMPU();
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitDebugConsole();
 
flexspi_nor_flash_init(EXAMPLE_FLEXSPI);
 
PRINTF("\r\nFLEXSPI example started!\r\n");
 
/* Get vendor ID. */
status = flexspi_nor_get_vendor_id(EXAMPLE_FLEXSPI, &vendorID);
if (status != kStatus_Success)
{
return status;
}
PRINTF("Vendor ID: 0x%x\r\n", vendorID);
 
#if !(defined(XIP_EXTERNAL_FLASH))
/* Erase whole chip . */
PRINTF("Erasing whole chip over FlexSPI...\r\n");
 
status = flexspi_nor_erase_chip(EXAMPLE_FLEXSPI);
if (status != kStatus_Success)
{
return status;
}
PRINTF("Erase finished !\r\n");
 
#endif
 
/* Enter quad mode. */
status = flexspi_nor_enable_quad_mode(EXAMPLE_FLEXSPI);
if (status != kStatus_Success)
{
return status;
}
 
/* Erase sectors. */
PRINTF("Erasing Serial NOR over FlexSPI...\r\n");
status = flexspi_nor_flash_erase_sector(EXAMPLE_FLEXSPI, EXAMPLE_SECTOR * SECTOR_SIZE);
if (status != kStatus_Success)
{
PRINTF("Erase sector failure !\r\n");
return -1;
}
 
memset(s_nor_program_buffer, 0xFFU, sizeof(s_nor_program_buffer));
 
DCACHE_InvalidateByRange(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE, FLASH_PAGE_SIZE);
 
memcpy(s_nor_read_buffer, (void *)(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE),
sizeof(s_nor_read_buffer));
 
if (memcmp(s_nor_program_buffer, s_nor_read_buffer, sizeof(s_nor_program_buffer)))
{
PRINTF("Erase data -  read out data value incorrect !\r\n ");
return -1;
}
else
{
PRINTF("Erase data - successfully. \r\n");
}
 
for (i = 0; i < 0xFFU; i++)
{
s_nor_program_buffer[i] = i;
}
 
status =
flexspi_nor_flash_page_program(EXAMPLE_FLEXSPI, EXAMPLE_SECTOR * SECTOR_SIZE, (void *)s_nor_program_buffer);
if (status != kStatus_Success)
{
PRINTF("Page program failure !\r\n");
return -1;
}
 
DCACHE_InvalidateByRange(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE, FLASH_PAGE_SIZE);
 
memcpy(s_nor_read_buffer, (void *)(EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE),
sizeof(s_nor_read_buffer));
 
if (memcmp(s_nor_read_buffer, s_nor_program_buffer, sizeof(s_nor_program_buffer)) != 0)
{
PRINTF("Program data -  read out data value incorrect !\r\n ");
return -1;
}
else
{
PRINTF("Program data - successfully. \r\n");
}
 
while (1)
{
}
}

 

status_t flexspi_nor_enable_quad_mode(FLEXSPI_Type *base)
{
flexspi_transfer_t flashXfer;
status_t status;
uint32_t writeValue =0x0200;// FLASH_QUAD_ENABLE;

#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
flexspi_cache_status_t cacheStatus;
flexspi_nor_disable_cache(&cacheStatus);
#endif

/* Write enable */
status = flexspi_nor_write_enable(base, 0);

if (status != kStatus_Success)
{
return status;
}

/* Enable quad mode. */
flashXfer.deviceAddress = 0;
flashXfer.port = FLASH_PORT;
flashXfer.cmdType = kFLEXSPI_Write;
flashXfer.SeqNumber = 1;
flashXfer.seqIndex = NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG;
flashXfer.data = &writeValue;
// flashXfer.dataSize = 1;
flashXfer.dataSize = 2;


status = FLEXSPI_TransferBlocking(base, &flashXfer);
if (status != kStatus_Success)
{
return status;
}

status = flexspi_nor_wait_bus_busy(base);

/* Do software reset. */
FLEXSPI_SoftwareReset(base);

#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
flexspi_nor_enable_cache(cacheStatus);
#endif

return status;
}

@kerryzhou @michael_imxrt @IMXRT1050 

 

0 Kudos
Reply