MIMXRT1052DVL6A Vs MIMXRT1052DVL6B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1052DVL6A Vs MIMXRT1052DVL6B

ソリューションへジャンプ
1,565件の閲覧回数
guitardenver
Contributor IV

Hello,

I am looking the the IMX RT series Crossover MCUs.

The datasheets seems to imply they are the same thing, just the "DVL6B" is the latest revision of the silicon.

Capture.PNG

 

1) Could you comment on the differences between the two? Or put a link to a document that describes the differences?

2) Is the "DVL6A" going to remain in full production? Or will "DVL6B" have to take over soon?

Thanks,

Matt

0 件の賞賛
返信
1 解決策
1,518件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Matt,

Please check AN12146. The DVL6A is finished. Only DVL6B can provide to customer.

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,519件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Matt,

Please check AN12146. The DVL6A is finished. Only DVL6B can provide to customer.

Regards,

Jing

0 件の賞賛
返信