MIMXRT1024 Linux DTS for GPIO interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1024 Linux DTS for GPIO interrupt

Jump to solution
2,479 Views
sbabu
Contributor III

Hi All,

I want to use GPIO_SD_B1_05 to 08 (GPIO port 3 ) as interrupts which will trigger a interrupt on raising edge on MIMXRT1024 running Linux. Can anybody please share any reference DTS file to achieve the same. Do I need to make any other changes in driver etc other than the DTS entry. Thanks in advance.

Regards,

Babu

 

 

 

Labels (2)
0 Kudos
Reply
1 Solution
2,450 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sbabu ,

  Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.

  Or your use the linux gcc to compile the RT1024 code?

   Until now, we still don't have the linux DTS for the RT1024.

 

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
2 Replies
2,451 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sbabu ,

  Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.

  Or your use the linux gcc to compile the RT1024 code?

   Until now, we still don't have the linux DTS for the RT1024.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply
2,444 Views
sbabu
Contributor III

Hi 

@kerryzhou - Thanks. No worries. We will check on it.

0 Kudos
Reply