MIMXRT1024 Linux DTS for GPIO interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1024 Linux DTS for GPIO interrupt

ソリューションへジャンプ
2,471件の閲覧回数
sbabu
Contributor III

Hi All,

I want to use GPIO_SD_B1_05 to 08 (GPIO port 3 ) as interrupts which will trigger a interrupt on raising edge on MIMXRT1024 running Linux. Can anybody please share any reference DTS file to achieve the same. Do I need to make any other changes in driver etc other than the DTS entry. Thanks in advance.

Regards,

Babu

 

 

 

ラベル(2)
0 件の賞賛
返信
1 解決策
2,442件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sbabu ,

  Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.

  Or your use the linux gcc to compile the RT1024 code?

   Until now, we still don't have the linux DTS for the RT1024.

 

Wish it helps you!

Best Regards,

Kerry

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,443件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sbabu ,

  Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.

  Or your use the linux gcc to compile the RT1024 code?

   Until now, we still don't have the linux DTS for the RT1024.

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信
2,436件の閲覧回数
sbabu
Contributor III

Hi 

@kerryzhou - Thanks. No worries. We will check on it.

0 件の賞賛
返信