MIMXRT1024 GPIO interrupt mapping on ucLinux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1024 GPIO interrupt mapping on ucLinux

1,248 Views
sbabu
Contributor III

Dear All,

On IMXRT1024 GPIO port3 has 84 as interrupt assigned by micro controller. So I can have a single ISR for 16 GPIOs. But on ucLinux its giving separate interrupt for each GPIO. So I need separate handlers. Is there a way to get a  single interrupt like in MCUXpresso SDK example in Linux?

Thanks,

babu

Labels (2)
0 Kudos
Reply
1 Reply

1,203 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If you are in iclinux you have to follow the interrupt as it declares, now we do not have any project for rt1024 in linux but MCUXpresso have an example on this GPIO.

 

Regards

0 Kudos
Reply