MIMXRT1020_EVK Design files .alg file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1020_EVK Design files .alg file

1,107件の閲覧回数
fycevher
Contributor I

I want to import layout of MIMXRT1020_EVK which is LAY-29857_B1.brd to Altium Designer. Since I have no Allegro license I need .alg file.

 

Could you please help me about it?

 

Regards 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,097件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could you please help me with it?
-- Unfortunately, we don't provide it, as I know, the Altium Designer support to import the brd file, maybe you can give it a try.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信

1,089件の閲覧回数
fycevher
Contributor I

@jeremyzhou 

As far as I know, Altium Designer can import .brd files in two ways; firstly, Allegro license should be available. secondly, .alg files can be used without Allegro license. I have no Allegro license. Therefore, I need ASCII (.alg) files. 

 

In this topic, Yuri sent .alg file to solve the same problem. Please help me!

Good bye!

0 件の賞賛
返信