MIMXRT1020 DMA bus error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMXRT1020 DMA bus error

1,345 次查看
SatPDG
Contributor II

Hi,

I am working on an embedded project that uses the MIMXRT1020. In the project, we have a sampling chain that uses the internal ADC at a speed of around 300kHz. The sampling chain looks like this : The PIT triggers the ADC_ETC that triggers the DMA when the conversion is complete. When the DMA has stored 256 samples, a software interrupt is triggered to allow the transfer of these buffer to a bigger buffer. When 10 DMA buffer has been received, the DMA interrupt calls a function. This function is executed every 8.5 ms ((256*10)/300k = 8.5 ms).

At each 500 ms, another task, the task 2, executes some calculation over some other big buffer. The computation takes around 20 ms to execute. Some FFT and buffer transfer are done during the computation. We realized that during the 20 ms of computation, the function, call by the DMA interrupt, is not called every 8.5 ms but at a higher time delay. We suspect that it could be a bus problem. With all the load and store done in the task 2 we think that all the RAM access of the task may delay some DMA transfer. When we stop the task 2, there is no delay in the function call.

We have read about the bus in the system and tried to reorganize the buffer location in the different system's RAM, but it did not change anything. Here what we understood :

1) The DMA is connected to the IP bus.

2) The OCRAM is connected to the AXI64 bus.

3) The ITCM and DTCM are connected to the TCM interface.

Could it be possible to place the DMA buffer in the OCRAM and the task's buffer in the DTCM or the ITCM so that, when the ARM core executes a load or store, it does not use the AXI64 bus? During this time, the IP bus and the AXI64 bus would be used by the DMA to write the sample in the OCRAM? Is there another memory configuration that could help use achieved what we want to do? Is there a way to give priority to the DMA transfers?

I cannot but the code in the forum, but I would be happy to share it under a NDA agreement.

Thank you

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,242 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @SatPDG 

 

Please accept our apologies for the long delay on having an answer for your.

Hopefully you find well, and hopefully you still need the information requested, my suggestion for your concerns is to take a view on AN12437 (https://www.nxp.com/docs/en/application-note/AN12437.pdf) to enhance the performance on reading from OCRAM, and those are changes that you can do on Hardware to improve read speed.

 

Regarding your question: "Is there a way to give priority to the DMA transfers?"

-DMA transfers have the highest priority, just behind ResetISR, so the delay that you are presenting, is by the jump from DMA ISR to the function called, that it takes aproximately 12 clock cycles to jump, more clock cycles to execute the function and another 12 clock cycles to come back and clear the isr flag.

 

Hope this information was helpful, please let me know if you have more questions.

 

 

BR.
Pablo Avalos.

 

0 项奖励
回复

1,304 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @SatPDG 

 

Thanks a lot for being so patient on this ticket.

 

I am now handling this case and I would like to ask for you some more time to have an accurate answer to your issue by doing some tests and double-reviewing.

 

Appreciating so much your patience, I will look forward and then get back to you with a feedback.

 

Thanks a lot!

 

Best Regards.
Pablo Avalos.

0 项奖励
回复