MIMX9302CVVXDAB power consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMX9302CVVXDAB power consumption

971 Views
m_hjelm
Contributor I

Hi, 

I am looking for better data on the powerconsumption of the rails for the MIMX9302CVVXDAB

Since it is clocked down (900MHz) i expect the current to be lower. Not sure thou if i can apply lower voltage to the VDD SOC as well. 

The DDR interface is also running at a lower speeed. 

So basically a full load measurement so that i can design a Power solution for it. 

And no using the PMIC is not an option. I have a 3.3v rail and that will not change so the PMIC cannot be used. 

Has anyone done these kind of measurements?

 

 

Tags (1)
0 Kudos
Reply
3 Replies

939 Views
m_hjelm
Contributor I

Yes i have read the app note many times but i cannot find any power requirement when running the device on 900MHz, which is the only possibility of that device as well as reduced DDR speed, and full load. I do not think idle is the right test for designing the PoL of the system. 

0 Kudos
Reply

931 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @m_hjelm!

 

We refer to Low Drive Mode when the processor operates at 900 MHz.

All values labeled as "Low Drive Mode" in the application note correspond to the processor running at 900 MHz.

Please refer to the following table for the naming conventions we use for each processor frequency.

 

Chavira_0-1750339445910.png

 

Best Regards!

Chavira

0 Kudos
Reply

947 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @m_hjelm!

Thank you for reaching out to NXP Support!

 

You can refer to Application Note AN13917, where we present a variety of use cases along with their corresponding current consumption measurements.

 

Best regards,
Chavira

0 Kudos
Reply