MIMX8MQ6CVAHZAB || Use Case support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMX8MQ6CVAHZAB || Use Case support

4,377 次查看
JyotiVaishnav
Contributor II

Hello NXP team, 

We are using a part MIMX8MQ6CVAHZAB in our design. 

We have a use case of 4 Camera Decode (1080p30) +  Compute (Offloaded to AI Accelerator) + CPU Post processing (overlay / bounding box) + Composite view to the display.

Along with the above use case if the encoding is also required, do you have any recommendations of an SoC in the iMX8 Family?

0 项奖励
回复
9 回复数

4,294 次查看
jimmychan
NXP TechSupport
NXP TechSupport
0 项奖励
回复

4,289 次查看
JyotiVaishnav
Contributor II

Hello @jimmychan 

Thanks!

i.MX8QM - It is an high rated processor. 

i.MX 8M Quad or i.MX 8M Plus Quad out of this two processor any one can meet our requirements? 

0 项奖励
回复

4,247 次查看
jimmychan
NXP TechSupport
NXP TechSupport

i.MX8MP is better. It has NPU for machine learning task. 2 x MIPI-CSI could connect two cameras. Other cameras could connect via Network (IP cameras to GB Ethernet on 8MP) and USB could connect one. 

0 项奖励
回复

4,190 次查看
JyotiVaishnav
Contributor II

Hello @jimmychan 

Thanks for the feedback. 

We need to know the some more information on our use case.

Use Case :  

  1. Max Decode :
    1x1080P60 (H265 & H264)
    2 x 1080P30 (H265 & H264)
    4 x 1080P15 (H265 & H264)
    4 x 720P30 (H265 & H264)
  2. Max Decode :
    1x1080P60 (H265 & H264)
    2 x 1080P30 (H265 & H264)
    4 x 1080P15 (H265 & H264)
    4 x 720P30 (H265 & H264)

 

  1. Compute (Offloaded to AI Accelerator) 
  2. CPU Post processing (overlay / bounding box) + Composite view to the display.

 

Can you please share the below details : 

Minimum DDR & eMMC size requirement with respect to the above mentioned use case.

0 项奖励
回复

4,161 次查看
jimmychan
NXP TechSupport
NXP TechSupport

It depends which OS will you using. There are Android and Linux BSP. And what kind of application will you run on your system to capture and compute the data. So it is better to buy the i.MX8MP EVK to develop and run your applications on it. It would more accurate to check how many memory and EMMC spaces will need for your use cases.

0 项奖励
回复

4,187 次查看
JyotiVaishnav
Contributor II

Hello @jimmychan 

We want to know one more thing, According to our use case which is the best suitable processor for our design. 

out of below two process which is the best suitable for our design. 

MIMX8ML8CVNKZAB

MIMX8ML6CVNKZAB

Your feedback is important for us. 

 

0 项奖励
回复

4,160 次查看
jimmychan
NXP TechSupport
NXP TechSupport

jimmychan_0-1695781362948.pngjimmychan_0-1695781362948.png

This table is in the datasheet. Do you need the NPU? if need, then select the part number that include the NPU.

0 项奖励
回复

4,295 次查看
jimmychan
NXP TechSupport
NXP TechSupport

So, what is the requirement of the encoding?

0 项奖励
回复

4,340 次查看
JyotiVaishnav
Contributor II

Hello NXP Team, 

Can you please update on use case support.

 

0 项奖励
回复