MIMX8MM6DVTLZAA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMX8MM6DVTLZAA

Jump to solution
6,167 Views
Arek
Contributor I

I bought a microcontroller but I was wrong because I ordered it with a narrow temperature range. Can anyone answer me, what's the difference with the MPU with the range of -40-85st C ?.

 

Best regards

Arek

Sat-Tech

0 Kudos
Reply
1 Solution
6,159 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hi Arek,

 

There's no difference.

Best Regards.

View solution in original post

0 Kudos
Reply
2 Replies
6,160 Views
Juan-Rodarte
NXP Employee
NXP Employee

Hi Arek,

 

There's no difference.

Best Regards.

0 Kudos
Reply
6,156 Views
Arek
Contributor I

I am wondering if the processor will be able to work in a wider temperature range than the manufacturer writed?
The purchased MIMX8MM6DVTLZAA processors have a temperature range of 0-95 degrees C and I need from  -10 to 100 degrees C.
The appropriate one would be MIMX8MM6CVTLZAA, I bought 150 pcs of modules Somlab with this processor with low temperature range.

Best Regards
Arek Kochański+48609721072
Sat-Tech
farm24.io/home

0 Kudos
Reply