MIMX8MM6DVTLZAA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,175件の閲覧回数
Arek
Contributor I

I bought a microcontroller but I was wrong because I ordered it with a narrow temperature range. Can anyone answer me, what's the difference with the MPU with the range of -40-85st C ?.

 

Best regards

Arek

Sat-Tech

0 件の賞賛
返信
1 解決策
6,167件の閲覧回数
Juan-Rodarte
NXP Employee
NXP Employee

Hi Arek,

 

There's no difference.

Best Regards.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
6,168件の閲覧回数
Juan-Rodarte
NXP Employee
NXP Employee

Hi Arek,

 

There's no difference.

Best Regards.

0 件の賞賛
返信
6,164件の閲覧回数
Arek
Contributor I

I am wondering if the processor will be able to work in a wider temperature range than the manufacturer writed?
The purchased MIMX8MM6DVTLZAA processors have a temperature range of 0-95 degrees C and I need from  -10 to 100 degrees C.
The appropriate one would be MIMX8MM6CVTLZAA, I bought 150 pcs of modules Somlab with this processor with low temperature range.

Best Regards
Arek Kochański+48609721072
Sat-Tech
farm24.io/home

0 件の賞賛
返信