MFGtool : /dev/utp missing in kernel rootfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFGtool : /dev/utp missing in kernel rootfs

1,744 次查看
anush_deekonda
Contributor I

 Hi,

I am using Yocto Sumo version.

The kernel boots up on yocto setup but there is no /dev/utp device node in the rootfs.

1. what kernel configuration need to be done inorder to create "/dev/utp" at boot up?

2. Also what is the major minor numbers of /dev/utp device node.

i am trying "uuc /dev/utp" which is not working.

3. Also the MFG tool on windows gets disconnected on kernel boot up on the yocto setup.

Is this expected behavior before launching uuc /dev/utp?

 

Thank you,

Anush D.

#mfgtools‌

#yocto-project‌

#fsl_utp‌

标签 (2)
0 项奖励
回复
1 回复

1,708 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Anusha

one can look at latest mfg tool release, Rocko

Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX6,7 BSP

mfg tool is not more supported recommended to migrate to uuu tool

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复