MFGtool : /dev/utp missing in kernel rootfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGtool : /dev/utp missing in kernel rootfs

1,697件の閲覧回数
anush_deekonda
Contributor I

 Hi,

I am using Yocto Sumo version.

The kernel boots up on yocto setup but there is no /dev/utp device node in the rootfs.

1. what kernel configuration need to be done inorder to create "/dev/utp" at boot up?

2. Also what is the major minor numbers of /dev/utp device node.

i am trying "uuc /dev/utp" which is not working.

3. Also the MFG tool on windows gets disconnected on kernel boot up on the yocto setup.

Is this expected behavior before launching uuc /dev/utp?

 

Thank you,

Anush D.

#mfgtools

#yocto-project

#fsl_utp

ラベル(2)
0 件の賞賛
返信
1 返信

1,661件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anusha

one can look at latest mfg tool release, Rocko

Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX6,7 BSP

mfg tool is not more supported recommended to migrate to uuu tool

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信