MFGtool MultiPanel is not loading the uboot properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGtool MultiPanel is not loading the uboot properly

2,683件の閲覧回数
dibing
Contributor I

Hi,

we have designed a Vehicle Automotive system with using NXP iMX6Q processor in Sabre platform. We are using eMMC and SD card as boot devices.

Here we are using MFGtool for ubooting the cpu and this is the first time with MFGtool

we have selected the "mfgtool2-android-mx6dqscm-1gb-qwks-rev2-sd.vbs" and started the ubooting after connecting the USB otg port of our board to USB port of HOST computer.

But, after loading kernal the MFGtool Multipanel is showing "Loading U-boot" and no further changes in the screen. There is no console in UART also. 

But we are getting console in the Linux system using Usb loader.

How can I solve the problem with MFGTOOL ??

** I have attached the MfgTool_MultiPanel window here

タグ(1)
0 件の賞賛
返信
1 返信

2,416件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

please make sure you are selecting the proper vbs file that match your board.

the main script of mfgtool is ucl2.xml. Basically, the vbs file + cfg.ini are used to setup the variables in the script. You can modify the script content directly to match your board and the filename of images. Please let me know if you have any question about the script.

0 件の賞賛
返信