MFGTool2 get MAC address on error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFGTool2 get MAC address on error

633 次查看
Alex_S
Contributor I

I am using MFGTool2 (ucl2.xml) for burning 4 devices at the same time. I would like to get the MAC address of the device if any of the processes does not success. I have tried to obtain the MAC address on a .txt before and after the proccess to compare it later with the following comand:

<CMD state="Updater" type="push" body="read [.txt with the MAC]" savedfile="MAC.txt">Obtaining MAC</CMD>

Since the 4 processes happen paralelly the .txt is overwritten resulting in only the last MAC address. I have not found much info of ucl2 commands.

So is it possible to just append the MAC instead of overwrite it to the .txt or just to get the .txt when an error occurs?

Thanks

标签 (1)
0 项奖励
回复
0 回复数