MFGTool error while writing boot.img

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGTool error while writing boot.img

1,078件の閲覧回数
Anerudh
Contributor I

Hi all,

 

I am trying to boot an android prebuilt image on the IMX6Q board with the MFG tool. The android version I am trying to boot is android 6 (android_M6.0.1_2.1.0). I have placed the necessary image files inside the directory "C:\Users\rise\Music\android_L5.0.0_1.0.0-ga_tools\mfgtools\Profiles\Linux\OS Firmware\files\android\sabresd". 

The tool gives an error while writing the boot.img and the MGFTool log file gives the following : 

ModuleID[2] LevelID[1]: PortMgrDlg(0)--MSCDevice--Command Push(no file) excute failed
ModuleID[2] LevelID[10]: CmdOperation[0], current command executed failed, so SetEvent(hDevCanDeleteEvent)

 

Does anybody know how to solve this issue? What should I do to boot the prebuilt image in the board?

Regards

0 件の賞賛
返信
1 返信

1,054件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP reference board or the board you design yourself? And have you using the proper images for your board?

0 件の賞賛
返信