MFGTOOL V2 support on IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGTOOL V2 support on IMX6

2,084件の閲覧回数
tomsaluzzo
Contributor III

Using the MCIMX6Q7CZK08AD.

Is there any way to verify if the latest MFGTOOL V2 will work with this pop processor? We keep running into issues where it’s not able to write to the DDR2.

ラベル(1)
0 件の賞賛
返信
1 返信

1,755件の閲覧回数
b36401
NXP Employee
NXP Employee

Actually MfgTool2 is official Manufacturing Toolkit for i.MX6Q. Here are download links for Linux 3.10.17 and 4.1.15 respectively:
http://nxp.com/webapp/Download?colCode=IMX_6_MFG_L3.10.17_1.0.0_TOOL
http://nxp.com/webapp/Download?colCode=IMX6_L4.1.15_1.0.0_MFG_TOOL

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信