MFGTOOL V2 support on IMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFGTOOL V2 support on IMX6

2,070 次查看
tomsaluzzo
Contributor III

Using the MCIMX6Q7CZK08AD.

Is there any way to verify if the latest MFGTOOL V2 will work with this pop processor? We keep running into issues where it’s not able to write to the DDR2.

标签 (1)
0 项奖励
回复
1 回复

1,741 次查看
b36401
NXP Employee
NXP Employee

Actually MfgTool2 is official Manufacturing Toolkit for i.MX6Q. Here are download links for Linux 3.10.17 and 4.1.15 respectively:
http://nxp.com/webapp/Download?colCode=IMX_6_MFG_L3.10.17_1.0.0_TOOL
http://nxp.com/webapp/Download?colCode=IMX6_L4.1.15_1.0.0_MFG_TOOL

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复