MFG toolv2 for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG toolv2 for imx6q

Jump to solution
3,096 Views
小樺陳
Contributor I

hi:

   i download:android_L5.0.0_1.0.0-ga_tools.tar.gz and android_L5.0.0_1.0.0-ga_images_6qsabresd.tar.gz .

  1. i copy android_L5.0.0_1.0.0-ga_full_image_6qsabresd\SD\*  to mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware

  2. i copy android_L5.0.0_1.0.0-ga_full_image_6qsabresd\u-boot-imx6q.imx(change name u-boot-imx6qsabresd_sd.imx) to  mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware

  3.Mfg tool_MutiPanel will pending after press start buttonerror.bmp

cfg.ini:

[profiles]

chip = Linux

[platform]

board = SabreSD

[LIST]

name = SDCard

[variable]

board = sabresd

mmc = 0

sxuboot=17x17arm2

sxdtb=17x17-arm2

ldo=

MfgTool.log:

DLL version: 2.3.3

Thursday, December 31, 2015 15:29:21   Start new logging

ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[00DCEAA0]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[00DD7090]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[00DDCA90]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[00DE2080]

ModuleID[2] LevelID[10]: Device Manager thread is running

ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is F:\task\android\5.0.0\mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware\u-boot-imx6qsabresd_sd.imx

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is F:\task\android\5.0.0\mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware\zImage, address is 0x12000000

ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is F:\task\android\5.0.0\mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware\fsl-image-mfgtool-initramfs-imx6qdlsolo.cpio.gz.u-boot, address is 0x12C00000

ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: ExecuteCommand--Load[WndIndex:0], File is F:\task\android\5.0.0\mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware\zImage-imx6q-sabresd.dtb, address is 0x18000000

ModuleID[2] LevelID[10]: PortMgrDlg(0)--Command Load excute successfully, retry count: 0

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: CmdOperation[0], skip current command, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: ExecuteCommand--Jump[WndIndex:0]

ModuleID[2] LevelID[10]: *********MxHidDevice[00DE2080] Jump to Ramkernel successfully!**********

ModuleID[2] LevelID[10]: CmdOperation[0], current state command has been finished and the last command is successful, so SetEvent(hDevCanDeleteEvent)

ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is F:\task\android\5.0.0\mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware\u-boot-imx6qsabresd_sd.imx

Labels (1)
0 Kudos
Reply
1 Solution
2,465 Views
vijaikumar
Contributor III

Hi,

    You need to copy the images you wish to flash into the following location.

mfgtools_5.0.0\Profiles\Linux\OS Firmware\files

mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware contains specialized firmware files for initializing MFGTool.

Regards

Vijai Kumar K

View solution in original post

0 Kudos
Reply
2 Replies
2,466 Views
vijaikumar
Contributor III

Hi,

    You need to copy the images you wish to flash into the following location.

mfgtools_5.0.0\Profiles\Linux\OS Firmware\files

mfgtools_5.0.0\Profiles\Linux\OS Firmware\firmware contains specialized firmware files for initializing MFGTool.

Regards

Vijai Kumar K

0 Kudos
Reply
2,465 Views
小樺陳
Contributor I

vijaikumar:

                    Thank you for your prompt reply.But (i copy android_L5.0.0_1.0.0-ga_full_image_6qsabresd\SD\*  to mfgtools_5.0.0\Profiles\Linux\OS Firmware\files)the result is still the same problem.Can once again help me?

                      i catch terminal information:

U-Boot 2014.04-00201-g9d7bf9b (May 05 2015 - 10:14:54)

CPU:  Freescale i.MX6Q rev1.5 at 792 MHz !

CPU:  Temperature 31 C, calibration data: 0x59e50169

Reset cause: POR

Board: MX6-SabreSD

I2C:  ready

DRAM:  1 GiB

MMC:  FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:  serial

Err:  serial

Found PFUZE100 deviceid=10,revid=21

unsupported boot devices

check_and_clean: reg 0, flag_set 0

Fastboot: Normal

SATA isn't buildin

Net:  FEC [PRIME]

Warning: failed to set MAC address

Boot from USB for mfgtools

Use default environment for mfgtools

Run bootcmd_mfg: <NULL>

=>

0 Kudos
Reply