MFG flash error on Android 7.1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG flash error on Android 7.1.2

2,831 Views
aravinthkumarja
Senior Contributor II

Hi All,

I'm working on imx6q Android 7.1.2 platform. On by board have 4GB internal emmc. so in "device-partitions.bpt" file size i have changed to 4GB. 

{
"settings": {
"disk_size": "4 GiB",
"disk_alignment": 1048576
},

As per your procedure I followed to flash the Android images by using MFG tool. But it stopped at "Formatting cache partition" level. 

I have attached MFG logs with this post. 

Can you please provide solutions for this as soon as possible. 

Regards,

Aravinth

Labels (3)
0 Kudos
Reply
3 Replies

2,435 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello aravinthkumar,

     For image of android71.1.2 , 4gb is not enough, please use 8GB eMMC.

Have a nice day!

TIC weidong

0 Kudos
Reply

2,435 Views
aravinthkumarja
Senior Contributor II

Hi weidong.sun‌,

I have tried with 8GB sd card. It's booting but it get stuck after few seconds.

Args:

Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:off video=mxcfb1:off video=mxcfb2:off vido=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleb
lank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled androidboot.serialno=1b2429d4ea997115 androidboot.storage_type=e
mmc

Bootlog:

EXT4-fs (mmcblk1p3): mounted filesystem with ordered data mode. Opts: barrier=1
EXT4-fs (mmcblk1p10): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk1p10): 1 truncate cleaned up
EXT4-fs (mmcblk1p10): recovery complete
EXT4-fs (mmcblk1p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
EXT4-fs (mmcblk1p4): Ignoring removed nomblk_io_submit option                                                          
EXT4-fs (mmcblk1p4): recovery complete                                                                                 
EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit                                 
EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: (null)                                           
file system registered                                                                                                 
using random self ethernet address                                                                                     
using random host ethernet address                                                                                     
zram0: detected capacity change from 0 to 314572800                                                                    
logd.auditd: start                                                                                                     
logd.klogd: 8102597334                                                                                                 
Adding 307196k swap on /dev/block/zram0.  Priority:-1 extents:1 across:307196k SS                                      
binder: 260:260 transaction failed 29189, size 0-0                                                                     
logd.daemon: reinit                                                                                                    
sabresd_6dq:/ # healthd: No battery devices found                                                                      
ERROR: v4l2 capture: slave not found! V4L2_CID_HUE                                                                     
ERROR: v4l2 capture: slave not found! V4L2_CID_HUE                                                                     
init: Service 'surfaceflinger' (pid 264) killed by signal 11                                                           
init: Service 'surfaceflinger' (pid 264) killing any children in process group                                         
init: Service 'zygote' is being killed...                                                                              
init: Service 'zygote' (pid 269) killed by signal 9
init: Service 'zygote' (pid 269) killing any children in process group
init: write_file: Unable to open '/sys/android_power/request_state': No such file or directory
init: write_file: Unable to write to '/sys/power/state': Invalid argument
init: Service 'audioserver' is being killed...
init: Service 'cameraserver' is being killed...
init: Service 'media' is being killed...

sabresd_6dq:/ #
sabresd_6dq:/ # ERROR: v4l2 capture: slave not found! V4L2_CID_HUE
ERROR: v4l2 capture: slave not found! V4L2_CID_HUE

sabresd_6dq:/ # init: Starting service 'zygote'...
init: Starting service 'audioserver'...
init: Starting service 'cameraserver'...
init: Starting service 'media'...
init: couldn't write 428 to /dev/cpuset/camera-daemon/tasks: No such file or directory
init: Starting service 'netd'...
init: Starting service 'surfaceflinger'...

*************************** Get Stuck **********************************

Can you help on this.!

Regards,

Aravinth

0 Kudos
Reply

2,435 Views
aravinthkumarja
Senior Contributor II

Hi weidong.sun‌,

I will try on 8GB card and it have any issue i will come back with this soon.

From which version of android we need a 8GB card.?

Update:

I found below line in your Android User Guide Document.

The minimum size of the SD card is 4 GB.

Regards,

Aravinth

0 Kudos
Reply