MFG Tools for Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG Tools for Linux

20,152 Views
netstv
Contributor II

I'm working on the iMX28 and was wondering if anyone has ported the Mfgtools to linux?  If not, we will be starting that effort shortly and I will let you know how it goes.

 

Thanks in advance.

-stv

Tags (1)
22 Replies

651 Views
netstv
Contributor II
Thanks Chris.. we did it already.  We ported the USB downloader app, as that's all we wanted... Took about 3/4 of a day.
0 Kudos
Reply

651 Views
ChrisWilliamson
Contributor III

Freescale has not ported the MfgTool to Linux and do not have plans to do so at this time.  I estimate it would be a big undertaking as there is a lot of Windows specific code. For example, there is a considerable amount of code that crawls through the registry to link a specific USB Port to a GUI Panel.

I would suggest starting off with an “updater” app that only tries to communicate with a single device. Most of the real work is done in Apps/MfgTool.exe/ OpUtpUpdate.cpp (ucl.xml command processing) and Libs/DevSupport/HidDevice.cpp (ROM) and Libs/DevSupport/ Volume.cpp (UTP/MSC - Linux file-stor gadget).

 

Chris

0 Kudos
Reply