MFG Tool is not detecting / ADB also not detecting via USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG Tool is not detecting / ADB also not detecting via USB

2,092 Views
bruno07eee
Contributor I

Hi All,


In detail  about the issue : (Platform - iMx6 sabresd)

1 . USB is working for Host/Mass storage (Mouse/Pendrive) But it is not working as a device

2 . PC is not detecting the board via USB(Even device manager, PC not able to recognize the usb)

3 . Hardware lines are proper which verified by probing the USB_ID line.

4 . Board is booting properly with last flashed images.

Please let us know how we can recover from this issue(Boot from emmc only is available)

Regards,

Bruno(bruno@zumisolutions.com)

Labels (1)
0 Kudos
Reply
6 Replies

1,950 Views
bruno07eee
Contributor I

Hi Igor,

Thanks for your quick response.

yes we have verified USB_ID is high and _VBUS line is powered(3.3volts)

Can you please suggest me that how i can proceed to rule out this issue.

Regards,

Bruno

0 Kudos
Reply

1,950 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

could you try connection with windows xp computer.

What is full processor marking, what mfg tools

version was used (link) ?

Best regards

igor

0 Kudos
Reply

1,950 Views
bruno07eee
Contributor I

Hi Igor,

I was using windows 7 and (We have around 6 development board)It is working with all the board except one board.

Is that fine for your question/ Still you need the mfg tool and environment details?

Note : Issue board was working fine and Issue occured after N number of reflashing the image via mfg tool

Please let me know if you need any details.

Regards,

Bruno

0 Kudos
Reply

1,950 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

if this just one board then this may be soldering issue,

one can resolder processor.

Best regards

igor

0 Kudos
Reply

1,950 Views
bruno07eee
Contributor I

Hi Igor,

Thanks for your update and Let me check with my hardware team for the same.

Hope i will update the root cause and the issue fixed notes here.

Regards,

Bruno

0 Kudos
Reply

1,950 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bruno

please check with oscilloscope that USB_ID is high and

USB_H1_VBUS or USB_OTG_VBUS are powered.

Recommended to look at i.MX6 System Development User’s Guide for usb items

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply