MFG Tool Fails. Help..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG Tool Fails. Help..

Jump to solution
2,529 Views
KeshavaGN
Contributor V

Hi all,

I'm trying to flash NAND using MFG tool. It fails frequently with following lines on hyperterminal :

PID:00400002 TID:01BF000E ERROR: c:\wince700\platform\common\src\soc\common_fsl_v3\uut\uutdrv\bot.cpp line 766: PID:00400002 TID:01BF000E UsbMsFn!BOT_HandleCBW: Invalid CBW signature

Error message on MFGTool displays:

failed to run command: type="push" body="send" file="files/NK.nb0" timeout="10" onError="" text="Sending NK.nb0 file." ,, Error code:-1

What is the reason for this error? and how i can solve it?

Thanks.

With regards,

Keshava G N


Labels (3)
0 Kudos
Reply
1 Solution
2,189 Views
Yuri
NXP Employee
NXP Employee

Looks like a hardware bug. Please check USB schematic, using design checklist and reference designs.

View solution in original post

0 Kudos
Reply
2 Replies
2,190 Views
Yuri
NXP Employee
NXP Employee

Looks like a hardware bug. Please check USB schematic, using design checklist and reference designs.

0 Kudos
Reply
2,189 Views
KeshavaGN
Contributor V