MFG TOOL issue in custom BOard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MFG TOOL issue in custom BOard

2,136 次查看
ranjithhebbar
Contributor II

Dear all,

We are using custom board based on i.mx6 quad processor with YOCTO 3.14.52 BSP. While flashing to spi or msd using custom firmware in MFG tool firmware kernel is hanging. I have attached the MFG tool log file. In hardware instead of ENET_OTG_ID they used GPIO_1 OTG_ID. For that mux changes and the gpr register changes are done. Please find the log and help.

U-Boot 2015.04 (Aug 26 2016 - 19:59:44)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 35 C
Reset cause: POR
Board: i.MX6Q Televic
I2C: ready
DRAM: 2 GiB
force_idle_bus: sda=0 scl=0 sda.gp=0x0 scl.gp=0x0
force_idle_bus: failed to clear bus, sda=0 scl=0
force_idle_bus: sda=0 scl=0 sda.gp=0x0 scl.gp=0x0
force_idle_bus: failed to clear bus, sda=0 scl=0
force_idle_bus: sda=0 scl=0 sda.gp=0x0 scl.gp=0x0
force_idle_bus: failed to clear bus, sda=0 scl=0
PMIC: PFUZE100 ID=0x10
NAND: 1024 MiB
MMC: FSL_SDHC: 0
SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 1 not found
PHY reset timed out
FEC [PRIME]
Error: FEC address not set.

Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x5c1170 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: initramfs
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 4399959 Bytes = 4.2 MiB
Load Address: 12c00000
Entry Point: 12c00000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800b8ac

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 3.14.52 (user@iw-hd-dtp-014-u1204) (gcc version 4.9.1 (GCC) ) #2 SMP PREEMPT Fri Aug 26 20:46:35 IST 2016
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 Quad Televic Board
cma: CMA: reserved 320 MiB at 6a000000
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @ee721000 s8320 r8192 d16256 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520720
Kernel command line: console=ttymxc3,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
Memory: 1734900K/2097152K available (7504K kernel code, 454K rwdata, 2600K rodata, 392K init, 433K bss, 362252K reserved, 270336K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
lowmem : 0x80000000 - 0xef800000 (1784 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x809e648c (10106 kB)
.init : 0x809e7000 - 0x80a49080 ( 393 kB)
.data : 0x80a4a000 - 0x80abbb60 ( 455 kB)
.bss : 0x80abbb6c - 0x80b2819c ( 434 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB
Switching to timer-based delay loop
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)
Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x107249d0 - 0x10724a28
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU2: Booted secondary processor
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU3: Booted secondary processor
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
Brought up 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
Use WDOG1 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1100 mV
vdd3p0: 2625 <--> 3400 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2400 mV
vddarm: 725 <--> 1450 mV at 1150 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV at 1175 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usbphy_nop1.10 supply vcc not found, using dummy regulator
usbphy_nop2.11 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.18
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 16384 (order: 4, 65536 bytes)
TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP: reno registered
UDP hash table entries: 1024 (order: 3, 32768 bytes)
UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 4292K (82c01000 - 83032000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
imx rpmsg driver is registered.
imx_busfreq busfreq.14: DDR medium rate not supported.
Bus freq driver module loaded
futex hash table entries: 1024 (order: 4, 65536 bytes)
bounce pool size: 64 pages
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 3508
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight.15 supply power not found, using dummy regulator
MIPI DSI driver module loaded
MIPI DSI driver module loaded
mxc_sdc_fb fb.16: err interface_pix_fmt!
mxc_sdc_fb fb.16: get mxcfb of property fail
mxc_sdc_fb: probe of fb.16 failed with error -2
mxc_sdc_fb fb.17: err interface_pix_fmt!
mxc_sdc_fb fb.17: get mxcfb of property fail
mxc_sdc_fb: probe of fb.17 failed with error -2
mxc_sdc_fb fb.18: err interface_pix_fmt!
mxc_sdc_fb fb.18: get mxcfb of property fail
mxc_sdc_fb: probe of fb.18 failed with error -2
mxc_sdc_fb fb.19: registered mxc display driver lcd
Console: switching to colour frame buffer device 100x30
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.2
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1375 mV
SW1C: 300 <--> 1875 mV at 1375 mV
SW2: 800 <--> 3300 mV at 3300 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 3300 mV at 3150 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 1500 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2500 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 2800 mV
VGEN6: 1800 <--> 3300 mV at 3300 mV
Serial: IMX driver
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
console [ttymxc3] enabled
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71
nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xd3
nand: Micron MT29F8G08ABACAH4
nand: 1024MiB, SLC, page size: 4096, OOB size: 224
gpmi-nand 112000.gpmi-nand: enable the asynchronous EDO mode 5
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
gpmi-nand 112000.gpmi-nand: driver registered.
m25p80 spi0.0: m25p32 (4096 Kbytes)
spi_imx 2008000.ecspi: probed
spi_imx 2014000.ecspi: probed
libphy: Fixed MDIO Bus: probed
CAN device driver interface
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unregistered net_device): Using random MAC address: be:73:2b:f0:b9:79
Master Slave GPIO value is one!!!!!!!!!1
libphy: fec_enet_mii_bus: probed
PASS MII init
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
lm75 2-0048: hwmon0: sensor 'tmp75c'
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
imx2-wdt: probe of 20c0000.wdog failed with error -16
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
ata1: SATA link down (SStatus 0 SControl 300)
ahci-imx 2200000.sata: no device found, disabling link.
ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
Galcore version 5.0.11.33433
mmc2: host does not support reading read-only switch. assuming write-enable.
mmc2: new high speed SDHC card at address 0007
mmcblk2: mmc2:0007 SS08G 7.21 GiB
mmcblk2: p1
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_vpu 2040000.vpu: VPU initialized
LED GPIO NUMBER is :106
LED GPIO NUMBER is :7
LED GPIO NUMBER is :8
LED major no 247

usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
fsl-asrc 2034000.asrc: driver registered
NET: Registered protocol family 26
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VGEN3: disabling
VGEN2: disabling
VGEN1: disabling
SWBST: disabling
SW4: disabling
regulator-dummy: disabling
imx mcc test is registered.
MASS storage Init*******
MASS STORAGE MESSAGE BIND FUNCTION***********************
USB FUNCTION INSTANCE !!!!!!!!!!!!!
Number of LUNs=8
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
Number of LUNs=1
LUN: removable file: (no medium)
Number of LUNs=1
random: nonblocking pool is initialized

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,757 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

one can check VDDUSB voltage at output LDO_USB (3.0V nom) with oscilloscope

to exclude processor physical damage. Also one can try to boot linux

with OTG_ID updated configuration to check if usb interface in device mode works ok.

Please boot from sd card, writing it using sect.4.3 Preparing an SD/MMC card to boot

attached Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复