MDIO read timeout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MDIO read timeout

2,333 Views
thepnimit
Contributor III

Hi

we have problem with PHY driver 

[ 11.057721] fec 5b040000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 11.092883] fec 5b040000.ethernet eth0: MDIO read timeout
[ 11.098371] ------------[ cut here ]------------
[ 11.103006] WARNING: CPU: 1 PID: 375 at drivers/net/phy/phy.c:716 phy_error+0x10/0x58
[ 11.110840] Modules linked in: crct10dif_ce
[ 11.115218] CPU: 1 PID: 375 Comm: kworker/u8:3 Tainted: G C 5.4.70 #4
[ 11.124681] Hardware name: CompuLab CL-SOM-iMX8X on SB-iMX8X (DT)
[ 11.130789] Workqueue: events_power_efficient phy_state_machine
[ 11.136715] pstate: 60000005 (nZCv daif -PAN -UAO)
[ 11.141508] pc : phy_error+0x10/0x58
[ 11.145087] lr : phy_state_machine+0x90/0x178
[ 11.149447] sp : ffff8000126dbd60
[ 11.152757] x29: ffff8000126dbd60 x28: ffff800011616000
[ 11.158072] x27: 0000000000000000 x26: ffff80001006bce8
[ 11.163388] x25: 0000000000000000 x24: 00000000ffffff92
[ 11.168706] x23: ffff0000794dc800 x22: 0000000000000005
[ 11.174022] x21: ffff0000794dcc38 x20: ffff0000794dc7e0
[ 11.179339] x19: ffff0000794dc800 x18: 0000000000000010
[ 11.184656] x17: 0000000000000000 x16: 0000000000000000
[ 11.189972] x15: ffff00007831f470 x14: ffffffffffffffff
[ 11.195289] x13: ffff8000926db8a7 x12: ffff8000126db8b0
[ 11.200606] x11: ffff800011631000 x10: ffff800011725328
[ 11.205923] x9 : 0000000000000000 x8 : ffff800011726000
[ 11.211239] x7 : ffff80001067bb78 x6 : 00000000159b1c45
[ 11.216556] x5 : 00ffffffffffffff x4 : 0000000000000000
[ 11.221873] x3 : ffff0000794dcc38 x2 : 0000000000000000
[ 11.227190] x1 : ffff00007831f000 x0 : ffff0000794dc800
[ 11.232510] Call trace:
[ 11.234963] phy_error+0x10/0x58
[ 11.238191] phy_state_machine+0x90/0x178
[ 11.242208] process_one_work+0x198/0x320
[ 11.246220] worker_thread+0x48/0x420
[ 11.249890] kthread+0xf0/0x120
[ 11.253033] ret_from_fork+0x10/0x18
[ 11.256610] ---[ end trace 0ff57ed249eee65b ]---

Thepnimit

0 Kudos
Reply
1 Reply

2,325 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thepnimit

 

reason may be wrong image, one can look at compulab design resources and post issue

on board vendor support portal

https://www.compulab.com/products/computer-on-modules/cl-som-imx8-nxp-i-mx-8-system-on-module-comput...

 

Best regards
igor

0 Kudos
Reply