MCIMX8QuadMax Boot-UP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCIMX8QuadMax Boot-UP

1,847 次查看
mehran_ali
Contributor I

Hi, 
I have i.MX QuadMax MEK CPU board, of which the CM4 core I want to use for a bare metal application.

As instructed by the Quick Start Guide I received along with the board, placed my image file in the SD Card and set the Bootmode switches to 001100 so that SDCard is used by the Boot-ROM for booting the system up.

The quick start guide also instructs to configure a terminal window(Teraterm) with parameters 

Baudrate: 115200

Data bits: 8

Stop bit: 1

Parity: None

Flow Control: None

and connect the board to PC acting as host in order to monitor the boot activity on the terminal with a micro-usb cable.

It does not mention the VCP drivers to install and eventually, no COM ports for serial communication are available to be configured in the terminal window.

There are 4 unrecognized devices visible though under the "Other devices" section in Device Manager by the name of "USB Serial Port".

Could someone please point me in a direction where I can find the drivers for this specific target or a detailed Boot process?

imx8quadmax‌imx8quadmax-boot‌imx8quadmax-drivers‌MCIMX8QM-CPU

0 项奖励
回复
1 回复

1,677 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You can try to refer to this https://community.nxp.com/docs/DOC-342719 , install the usb driver. If it does not work contact us.

0 项奖励
回复