MCIMX7SABRE Camera Module Specifications and HDMI Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX7SABRE Camera Module Specifications and HDMI Support

Jump to solution
1,562 Views
UbaidShafi
Contributor I

Hallo,

I want to use MCIMX7SABRE for testing MiPi cable using image sensor having capabilities of 8MP or higher(4K resolution). I have read the 'Quick Start Guide SABRE Board for Smart Devices' and it mentions we can use OV5640 but this is a 5MP camera.

Q) Do we have a sensor module with 8MP or higher (with free running clock output) that we can use with the MCIMX7SABRE?
Q) Does the HDMI port support HDMI2.0 or higher?

I am really looking forward for the answers. Thanks in advance.

Regards,
Ubaid Ahmed Shafi
Munich, Germany

0 Kudos
Reply
1 Solution
1,553 Views
joanxie
NXP TechSupport
NXP TechSupport

Q) Do we have a sensor module with 8MP or higher (with free running clock output) that we can use with the MCIMX7SABRE?

>refer to the imx7d reference manual,

MIPI CSI-2 controller and D-PHY:
• Supports 2 data lanes and 1 clock lane
• Maximum bit rate of 1.5 Gbps

so if you need 8MP camera, only can support 15fps max, you can check if your camera can meet this

Q) Does the HDMI port support HDMI2.0 or higher?

> current imx7d sabresd board uses SiI9022ACNU convert, I checked this chip which doesn't support HDMI 2.0, but you can use other convert chip to support this

View solution in original post

1 Reply
1,554 Views
joanxie
NXP TechSupport
NXP TechSupport

Q) Do we have a sensor module with 8MP or higher (with free running clock output) that we can use with the MCIMX7SABRE?

>refer to the imx7d reference manual,

MIPI CSI-2 controller and D-PHY:
• Supports 2 data lanes and 1 clock lane
• Maximum bit rate of 1.5 Gbps

so if you need 8MP camera, only can support 15fps max, you can check if your camera can meet this

Q) Does the HDMI port support HDMI2.0 or higher?

> current imx7d sabresd board uses SiI9022ACNU convert, I checked this chip which doesn't support HDMI 2.0, but you can use other convert chip to support this