MCIMX257CJN4A 12x12 Package Layout Reference Design/Recommendations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCIMX257CJN4A 12x12 Package Layout Reference Design/Recommendations

1,965 次查看
dvona
Contributor II

Greetings,

Does Anyone know of a reference design that has been created for the MCIMX257CJN4A (12x12 package).  All the SDK kits seem to be based on the larger package.  I have reviewed app note AN3951, but am looking for something specific to this package if possible, and preferrably with PCB layout files.

Thanks for your help.

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,800 次查看
dvona
Contributor II

Is there an IBIS model for this 0.5 mm pitch BGA device?  I have only found the senna.ibs for the larger 17x17 package.

Best Regards,

-Dan

0 项奖励
回复

1,800 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dan, yes there is ibis model for it, however

since it is not officially released, please enter help service

request ticket to obtain it internally.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,800 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dan,

as far as I know Freescale did not produce such reference design for 12x12 package .

0 项奖励
回复