MCF5372, observed distorted output using the model MCF5372LCVM240.ibs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCF5372, observed distorted output using the model MCF5372LCVM240.ibs

745 次查看
sms2
Contributor I

Hello Everyone,

Request to understand , the reason about the high overshoot/Undershoot, Ripple,Non monotonicity for the Address/Data ,SDRAM,CPU_CLK signal using the model "MCF5372LCVM240.ibs".

pad_rfc_33_01,20pF Drive Strength is the IO used.

FYI,  have replaced the controller and observed  the signal using different controller, the result looks acceptable.

Kindly help me to understand about the model.


0 项奖励
回复
1 回复

724 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, I do not see your mentioned overshoot/undershoot situation with attached IBIS file.

Hui_Ma_1-1663895807515.pngHui_Ma_2-1663895832519.png

Mike

0 项奖励
回复