Hi,
I'm using iMX8MP-evk, booted from SD. I wanted to change the MAC address of eth0. I changed the variable "ethaddr" by the u-boot command and saved with saveenv command as follows.
u-boot=> setenv ethaddr 00:50:c2:46:40:11
u-boot=> saveenv
Saving Environment to MMC... Writing to MMC(1)... OK
When I rebooted, following messages appeared
Net:
Warning: ethernet@30be0000 MAC addresses don't match:
Address in ROM is 00:04:9f:07:0e:d8
Address in environment is 00:50:c2:46:40:11
eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]
After deleting the ethaddr as follows
u-boot=> setenv ethaddr
u-boot=> saveenv
Saving Environment to MMC... Writing to MMC(1)... OK
following messages appeared
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]
What is ROM mentioned above?
How do I write the MAC address in ROM?
Thanks,
Hideo