M4 gcc i686 host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M4 gcc i686 host

2,775 Views
davidpatton
Contributor III

Anyone know where I can get a pre-compiled GCC for the ARM M4 Cortex, hosted on i686-Linux? Everything I can find is for x86_64-Linux host. Thanks!

Labels (1)
0 Kudos
Reply
3 Replies

2,709 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can use the following:

GNU Toolchain | GNU-RM Downloads – Arm Developer  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,709 Views
davidpatton
Contributor III

Thanks...but they only have the pre-built compiler for x86_64, not i686.

I hate the thought of it, but do you know if the source tarball is already configured to generate arm-none-eabi-gcc, et al?

0 Kudos
Reply

2,709 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You may try the following:

GNU Arm Embedded Toolchain project files : GNU Arm Embedded Toolchain 

Regards,

Yuri.

0 Kudos
Reply