Ltib installation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ltib installation error

Jump to solution
3,975 Views
weihuang
Contributor I

Hi

using ubuntu 14.04 32bit, The BSP version is L2.6.35_1.1.0_130130_source.tar.gz


./ltib

an error occurs


/usr/bin/ld: ElftosbAST.o: undefined reference to symbol 'powf@@GLIBC_2.0'

//lib/i386-linux-gnu/libm.so.6: error adding symbols: DSO missing from command line

collect2: error: ld returned 1 exit status

make[1]: *** [elftosb] Error 1

make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/elftosb-2.6.35.3-1.1.0/bld/linux'

make: *** [all] Error 2

error: Bad exit status from /home/wei/imx28/ltib/tmp/rpm-tmp.2071 (%build)

RPM build errors:

    Bad exit status from /home/wei/imx28/ltib/tmp/rpm-tmp.2071 (%build)


Labels (1)
0 Kudos
Reply
1 Solution
3,598 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
4 Replies
3,599 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
3,599 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi wei huang,

You can refer to the thread in our community:Compile L2.6.35_1.1.0_130130 for i.MX28 on Ubuntu 13.10 64bit OS.

Hope this can help you.
Have a great day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,599 Views
Yuri
NXP Employee
NXP Employee

You may find the solution on the following (IMX LTIB COMMON ERRORS) :

freescale | HalfaGeek


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,599 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi wei huang,

Which board are you using?

Best Regards

Dan

0 Kudos
Reply