Low Power Mode (System IDLE/Low Power IDLE)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low Power Mode (System IDLE/Low Power IDLE)

2,976件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I would like to confirm the Low power mode.

I refer to the IMX6ULLCEC Rev 1.2.

 

  1. Entering System IDLE

It is described at P29 4.1.6.2 Low Power Mode in as following.

"This is a mode that the CPU can automatically enter when there is no thread running."

Q1.

Is my following understanding correct?

The software does not need to do something explicitly for entering system IDLE mode.

 

Q2.

Is it possible to set the condition to enter the system IDLE?

 

  1. Entering Low Power IDLE

Q3.

How is it able to enter the Low power IDLE?

 

  1. Return from IDLE mode

Q4.

How is it able to return from IDEL mode?

 

Q5.

Is it able to return by GPIO port transition?

 

Q6.

Is it possible to return from the IDLE mode to the RUN mode by changing the A/D value?

(Is it able to return to RUN mode triggered by A/D?)

 

Best Regards,

Eishi SHIBUSAWA

ラベル(2)
0 件の賞賛
返信
1 返信

2,645件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

>Q1.Is my following understanding correct?

>The software does not need to do something explicitly for entering system IDLE mode.

no, software low power driver performing steps to enter system IDLE mode, for example

in linux one can refer to Chapter 21Low-level Power Management (PM) Driver attached Linux Manual.

 

>Q2. Is it possible to set the condition to enter the system IDLE?

condition is set by low power driver, linux driver decides when it should put processor in low power mode.

 

  1. Entering Low Power IDLE

>Q3. How is it able to enter the Low power IDLE?

  1. Return from IDLE mode

>Q4. How is it able to return from IDEL mode?

please refer to sect.18.5.3.2.1 Entering WAIT mode, 18.5.3.2.2 Exiting WAIT mode

i.MX6ULL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

 

>Q5. Is it able to return by GPIO port transition?

yes

 

>Q6.Is it possible to return from the IDLE mode to the RUN mode by changing the A/D value?

>(Is it able to return to RUN mode triggered by A/D?)

yes, please refer to p.406, sect.13.3.7 MCU Wait Mode Operation i.MX6ULL Reference Manual

"The ADC interrupt wakes the MCU when the compare condition is met."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信