Looking for example for SDMA from host memory to EIM target using dmaengine API on 3.0.35

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for example for SDMA from host memory to EIM target using dmaengine API on 3.0.35

2,960件の閲覧回数
jayakumar2
Contributor V

Hi,

 

I'm using a i.mx6sololite board with 3.0.35 kernel. I've got a working example for memory to memory SDMA working. But I have not been able to get SDMA to an EIM target address working.

 

I took the drivers/char/mxc_sdma_memcopy_test.c example and made the following mods:

        dma_m2m_config.direction = DMA_MEM_TO_DEV;

        dma_m2m_config.dst_addr_width = DMA_SLAVE_BUSWIDTH_2_BYTES;

        dmaengine_slave_config(dma_m2m_chan, &dma_m2m_config);

 

So I set DMA_MEM_TO_DEV since this was host to device DMA transfer. My EIM bus is configured for 16-bit width (this works with regular host read/write).

 

        sg_init_table(sg, 1);

        sg_set_buf(&sg[0], wbuf, SDMA_BUF_SIZE);

        ret = dma_map_sg(NULL, sg, 1, dma_m2m_config.direction);

        dma_m2m_desc = dma_m2m_chan->device->device_prep_slave_sg(dma_m2m_chan,sg, 1, dma_m2m_config.direction, 1);

 

Above is my host memory buffer. The wbuf is kzalloced memory. The intention is to have app ioctl and copy_from_userspace.

 

My target address is CS1 EIM. So I do:

        int FPGA_ADDR_BASE = 0x0C000000;

 

        rbuf = ioremap(FPGA_ADDR_BASE, 1024*1024);

        if(!rbuf) {

                printk("error rbuf !!!!!!!!!!!\n");

                return -1;

        }

        printk(KERN_ERR "got rbuf=0x%x\n", rbuf);

 

        sg_init_table(sg2, 1);

        sg_set_buf(&sg2[0], rbuf, SDMA_BUF_SIZE);

        ret = dma_map_sg(NULL, sg2, 1, dma_m2m_config.direction);

        printk(KERN_ERR "%s:%d ret=%d\n", __func__, __LINE__, ret);

        dma_m2m_desc = dma_m2m_chan->device->device_prep_slave_sg(dma_m2m_chan,sg2, 1, dma_m2m_config.direction, 0);

 

But this fails at this point because device_prep_slave_sg returns NULL. When I test, I get:

got rbuf=0xc0c00000

imx-sdma imx-sdma: load_address = 0

imx-sdma imx-sdma: wml = 0x00000000

imx-sdma imx-sdma: shp_addr = 0xbfbbbf60

imx-sdma imx-sdma: per_addr = 0x00000000

imx-sdma imx-sdma: event_mask0 = 0x00000000

imx-sdma imx-sdma: event_mask1 = 0x00000000

sdma_write:215

sdma_write:224

imx-sdma imx-sdma: setting up 1 entries for channel 1.

imx-sdma imx-sdma: load_address = 0

imx-sdma imx-sdma: wml = 0x00000000

imx-sdma imx-sdma: shp_addr = 0xbfbbbf60

imx-sdma imx-sdma: per_addr = 0x00000000

imx-sdma imx-sdma: event_mask0 = 0x00000000

imx-sdma imx-sdma: event_mask1 = 0x00000000

imx-sdma imx-sdma: entry 0: count: 1024 dma: 0x8a002000  intr

sdma_write:227

sdma_write:236 ret=1

sdma_write:239 m2m_desc=  (null)

 

I have not been able to figure out why the prep_slave_sg fails as the ioremaped CS1 address is a valid DMA target.

 

I have attached the source code in case I have made any incorrect assumptions about how this is supposed to work. I tried using dma_m2m_config.dst_addr = rbuf as I was unsure whether setting the sg2 scatterlist is the correct way to specify the destination address but that fails in the same way.

 

Does anyone have an example for SDMA from host to EIM CS1 that is known to work?

 

Thanks!

Original Attachment has been moved to: mxc_sdma_memcopy_test.c.zip

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,629件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jaya

one can look at patch below

android-imx6-kitkat/0370-ENGR00233569-Add-test-codes-for-SDMA-M2M-copy-using-.patch at master · rabe...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,629件の閲覧回数
jayakumar2
Contributor V

Hi Igor,

Thanks for your reply. But that is the same code (memory to memory SDMA) that I used as the starting point for my test. Please see the attachment as the test I'm doing is memory-to-EIM SDMA. As I mentioned, when I set the destination address in the sglist to be the ioremap-ed EIM address, then the prep_slave_sg fails out. This is why I was looking for a specific example that tests EIM SDMA rather than memory-to-memory.

Thanks!

0 件の賞賛
返信

1,629件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jaya

it should work with EIM too. Had you mapped EIM addresses

with mmu ?

Best regards

igor

0 件の賞賛
返信

1,629件の閲覧回数
jayakumar2
Contributor V

Hi Igor,

Yes, I ioremap-ed the EIM CS1 base address. I posted the code that I used in the message and also the complete code in the attachment. See above at line 46.

Thanks.

0 件の賞賛
返信