Looking for EB804 Application Processor Silicon Revision from 1.3 to 1.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Looking for EB804 Application Processor Silicon Revision from 1.3 to 1.4

1,154 次查看
Virviglaz
Contributor I

Hi,

Looking for a document

i.MX 6Solo/6DualLite Application Processor Silicon Revision 1.3 to 1.4 Comparison

Thanks is advance,

Pavel

标签 (2)
0 项奖励
回复
2 回复数

1,145 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,137 次查看
Virviglaz
Contributor I

Hi,

Thanks a lot for the provided links

We are actually looking for the revision comparison document between silicon v1.3 and v1.4

This is needed to fix the secured u-boot lockup that we are facing now.

We currently using u-boot and SPL from 2016.09 and after soldering new processor v1.4 (HAB v4.2) the SPL refuses to boot.

We see this messages:

HAB Configuration: 0xcc, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x2c 0x42 0x33 0x30 0xe1 0x1e
0x00 0x00 0x00 0x00 0x80 0x00 0x0b 0x00
0x00 0x00 0x00 0x02 0x00 0x00 0x00 0x20
0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
0x00 0x00 0x00 0x08 0x00 0x00 0x00 0x00
0x00 0x00 0x00 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_ENG_FAIL (0x30)
CTX = HAB_CTX_ENTRY (0xE1)
ENG = HAB_ENG_SNVS (0x1E)

We are on the way to update the u-boot to version 2020.01-rc1 and I hope it will just start working, but I would like to know the revision change details.

Thanks is advance,

0 项奖励
回复