Local Alpha Blending

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Local Alpha Blending

1,443件の閲覧回数
saurabh206
Senior Contributor III

Hi,

Our setup  is like data from android surface flinger is available "/dev/graphics/fb0"

We want to do overlay with CSI buffer which is written on "/dev/graphics/fb1"

We are able to get it working with global alpha and colour keying. But due to some limitation with our GUI we can not use global alpha.

But If I disable global alpha and enable the local alpha than data from /dev/graphics/fb1 is not display.

- Is it possible to do alpha blending using local alpha without colour keying?

- What is a significance of alpha_phy_addr0, alpha_phy_addr1 and alpha_in_pixel?

Thanks

Saurabh


0 件の賞賛
返信
0 返答(返信)