Linux reboot problem watchdog software reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux reboot problem watchdog software reset

1,636 次查看
nikhil_sahu2
Contributor III

Hi 

We are working on imx6sx custom board running yocto zeus on that. we are facing the reboot freeze issue sometime when we are doing the soft reboot.

Sometimes board reboot but sometimes it stuck once it called the watchdog.

As a fix, just commenting out the following in arch/arm/boot/dts/imx6sx-sdb.dtsi from the linux kernel

&wdog1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_wdog>;
// fsl,ext-reset-output;
};

It will make only the software reset. So whenever you reboot, you will have only software components restarting.

if that would be ok? For example, is there a strict requirement for Hardware reset, everytime when a user initiates a system restart. 

Should we have to move with this fix?

Thanks,

Nikhil

 

0 项奖励
回复
1 回复

1,621 次查看
jimmychan
NXP TechSupport
NXP TechSupport

I think you can comment out the "ext-reset-output" if you don't use the WDOG_B pin.

0 项奖励
回复