Linux reboot problem watchdog software reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux reboot problem watchdog software reset

2,184 Views
nikhil_sahu2
Contributor III

Hi 

We are working on imx6sx custom board running yocto zeus on that. we are facing the reboot freeze issue sometime when we are doing the soft reboot.

Sometimes board reboot but sometimes it stuck once it called the watchdog.

As a fix, just commenting out the following in arch/arm/boot/dts/imx6sx-sdb.dtsi from the linux kernel

&wdog1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_wdog>;
// fsl,ext-reset-output;
};

It will make only the software reset. So whenever you reboot, you will have only software components restarting.

if that would be ok? For example, is there a strict requirement for Hardware reset, everytime when a user initiates a system restart. 

Should we have to move with this fix?

Thanks,

Nikhil

 

0 Kudos
Reply
1 Reply

2,169 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think you can comment out the "ext-reset-output" if you don't use the WDOG_B pin.

0 Kudos
Reply