Linux reboot problem watchdog software reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux reboot problem watchdog software reset

2,241件の閲覧回数
nikhil_sahu2
Contributor III

Hi 

We are working on imx6sx custom board running yocto zeus on that. we are facing the reboot freeze issue sometime when we are doing the soft reboot.

Sometimes board reboot but sometimes it stuck once it called the watchdog.

As a fix, just commenting out the following in arch/arm/boot/dts/imx6sx-sdb.dtsi from the linux kernel

&wdog1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_wdog>;
// fsl,ext-reset-output;
};

It will make only the software reset. So whenever you reboot, you will have only software components restarting.

if that would be ok? For example, is there a strict requirement for Hardware reset, everytime when a user initiates a system restart. 

Should we have to move with this fix?

Thanks,

Nikhil

 

0 件の賞賛
返信
1 返信

2,226件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think you can comment out the "ext-reset-output" if you don't use the WDOG_B pin.

0 件の賞賛
返信