Linux ns-world

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux ns-world

1,795 Views
ailtonlopes
Contributor III

Hi, im working with the Trustzone on the IMX6QSD board and i wanted to ask id there's a way to use linux as non-secure in the board.
Kind regards, 

Ailton Lopes

Labels (2)
0 Kudos
Reply
2 Replies

1,640 Views
Yuri
NXP Employee
NXP Employee

Hello,

   customers can try the recent NXP Linux BSP L4.9.88, which supports Optee, but it

is not enabled by default. For how to enable it, see ReadMe.

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

Documentation - OP-TEE 

Regards,

Yuri.

0 Kudos
Reply

1,640 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the topic as below, hope helpful for you

https://community.nxp.com/message/650147 

0 Kudos
Reply