Linux kernel spi_async function don't work on iMX6. Kernel panic from spi_imx driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux kernel spi_async function don't work on iMX6. Kernel panic from spi_imx driver

1,622 次查看
alexanderlyasin
Contributor I

Hello! I have a board with "i.CORE RQS M6" module with i.MX6DQRM proc. The Linux kernel 3.0.35 linked with spi_imx Hello! I have a board with "i.CORE RQS M6" module with i.MX6DQRM proc. The Linux kernel 3.0.35 linked with spi_imx and with spi_bitbang. On this board are any devices on the spi bus. I made drivers (kernel modules) for those SPI-devices.
I need implement data transfer by spi_async function now. When I implemented transfer by spi_async instead spi_sync - I get kernel panic:
Listing in attachement

 

How can I resolve this problem?

Original Attachment has been moved to: kernel_panic.zip

0 项奖励
回复
1 回复

1,448 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please add "printk" into your driver to check where it stop.

0 项奖励
回复