Linux kernel hangs after allocating contiguous DMA memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux kernel hangs after allocating contiguous DMA memory

2,247 次查看
mihaitaivascu
Contributor III

Hello,

    I am trying to allocate contiguous DMA memory in device tree as I need to store 5MP camera frames and the dma_alloc_coherent would complain otherwise. Unfortunately after the DMA appol is allocated the kernel hangs

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.6.0-xilinx (mivascu@ubuntu) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Mon Aug 13 03:51:10 PDT 2018
[ 0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: Hurricane Telescope main board (7z035)
[ 0.000000] Ignoring memory range 0x0 - 0x10000000
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] Reserved memory: created CMA memory pool at 0x10000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node buffer@0, compatible id shared-dma-pool
[ 0.000000] Memory policy: Data cache writealloc

   I would appreciate any suggestion related to what could be the problem or how to debug it

Thanks,

      Mihaita

0 项奖励
回复
1 回复

1,974 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mihaita

as Linux version 4.6.0 is not officially supported nxp kernel, one can try with

mxp releases described on

i.MX Software|NXP 

also may be useful to check memory

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复