Linux hangs after "Mount-cache hash table entries: 512"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux hangs after "Mount-cache hash table entries: 512"

3,824 Views
jbd64
Contributor III

Hi,

I have troubles adapting linux for our custom board based on an i.mx6 Solo.

U-boot is working, but linux hangs after : Mount-cache hash table entries: 512

Here is the complete log (U-boot + linux) :

U-Boot 2009.08 (janv. 08 2014 - 18:16:22)

CPU: Freescale i.MX6 family TO1.1 at 792 MHz

Temperature:   41 C, calibration data 0x5744e269

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 198000000Hz

emi_slow clock: 99000000Hz

ddr clock     : 396000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6DL/Solo-MASTERLIGHT: unknown-board Board: 0x61011 [WDOG ]

Boot Device: MMC

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

*** Warning - bad CRC or MMC, using default environment

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

FEC: Link is down 0

*** ERROR: `ethaddr' not set

FEC: Link is down 0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35MasterLight_1A+

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3715744 Bytes =  3.5 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

[    0.000000] Initializing cgroup subsys cpuset

[    0.000000] Initializing cgroup subsys cpu

[    0.000000] Linux version 3.0.35MasterLight_1A+ (dacnis@VM-CCF) (gcc version 4.7.2 (GCC) ) #11 Wed Jan 8 18:47:09 CET 2014

[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

[    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

[    0.000000] Machine: Freescale i.MX 6Solo MasterLight Board

[    0.000000] Ignoring unrecognised tag 0x54410008

[    0.000000] MX6Q_SABRESD_RESERVE START

[    0.000000] MX6Q_SABRESD_RESERVE END

[    0.000000] Memory policy: ECC disabled, Data cache writeback

[    0.000000] MX6_MAP_IO START

[    0.000000] CPU identified as i.MX6DL/SOLO, silicon rev 1.1

[    0.000000] MX6_MAP_IO END

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

[    0.000000] Kernel command line: console=ttymxc0,115200n8 rdinit=/linuxrc enable_wait_mode=off

[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)

[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

[    0.000000] allocated 4194304 bytes of page_cgroup

[    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups

[    0.000000] Memory: 1024MB = 1024MB total

[    0.000000] Memory: 1027284k/1027284k available, 21292k reserved, 360448K highmem

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

[    0.000000]     DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

[    0.000000]     vmalloc : 0xea800000 - 0xf2000000   ( 120 MB)

[    0.000000]     lowmem  : 0xc0000000 - 0xea000000   ( 672 MB)

[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

[    0.000000]       .init : 0xc0008000 - 0xc004c000   ( 272 kB)

[    0.000000]       .text : 0xc004c000 - 0xc0733000   (7068 kB)

[    0.000000]       .data : 0xc0734000 - 0xc0775a30   ( 263 kB)

[    0.000000]        .bss : 0xc0775a54 - 0xc07f8330   ( 523 kB)

[    0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

[    0.000000] NR_IRQS:496 nr_irqs:496 496

[    0.000000] MX6_INIT_IRQ START

[    0.000000] MXC GPIO hardware

[    0.000000] MX6_INIT_IRQ END

[    0.000000] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

[    0.000000] Set periph_clk's parent to pll2_pfd_400M!

[    0.000000] MXC_Early serial console at MMIO 0x21f4000 (options '115200n8')

[    0.000000] bootconsole [ttymxc0] enabled

[    0.000000] Console: colour dummy device 80x30

[    0.252063] Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

[    0.340356] pid_max: default: 32768 minimum: 301

[    0.345185] Security Framework initialized

[    0.349353] AppArmor: AppArmor initialized

[    0.353571] Mount-cache hash table entries: 512

I inserted printk in the beginning and end of functions of my board setup code.

The functions map_io, init_irq, timer, reserve are called, but linux crashes before the call of my board_init function.

Can you help me searching the problem ?

Thank you.

Labels (2)
0 Kudos
Reply
2 Replies

2,725 Views
jbd64
Contributor III

Now I have a more detailed log of the error occuring in linux.

We can see a "Kernel panic - not syncing: Attempted to kill the idle task!" :

U-Boot 2009.08 (janv. 08 2014 - 18:16:22)

CPU: Freescale i.MX6 family TO1.1 at 792 MHz

Temperature:   40 C, calibration data 0x5744e269

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock     : 66000000Hz

ipg per clock : 66000000Hz

uart clock    : 80000000Hz

cspi clock    : 60000000Hz

ahb clock     : 132000000Hz

axi clock   : 198000000Hz

emi_slow clock: 99000000Hz

ddr clock     : 396000000Hz

usdhc1 clock  : 198000000Hz

usdhc2 clock  : 198000000Hz

usdhc3 clock  : 198000000Hz

usdhc4 clock  : 198000000Hz

nfc clock     : 24000000Hz

Board: i.MX6DL/Solo-MASTERLIGHT: unknown-board Board: 0x61011 [WDOG ]

Boot Device: MMC

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

*** Warning - bad CRC or MMC, using default environment

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

FEC: Link is down 0

*** ERROR: `ethaddr' not set

FEC: Link is down 0

## Booting kernel from Legacy Image at 10800000 ...

   Image Name:   Linux-3.0.35MasterLight_1A+

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3716408 Bytes =  3.5 MB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

[    0.000000] Initializing cgroup subsys cpuset

[    0.000000] Initializing cgroup subsys cpu

[    0.000000] Linux version 3.0.35MasterLight_1A+ (dacnis@VM-CCF) (gcc version 4.7.2 (GCC) ) #39 Thu Jan 9 15:56:08 CET 2014

[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

[    0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

[    0.000000] Machine: Freescale i.MX 6Solo MasterLight Board

[    0.000000] Ignoring unrecognised tag 0x54410008

[    0.000000] MX6Q_SABRESD_RESERVE START

[    0.000000] MX6Q_SABRESD_RESERVE END

[    0.000000] Memory policy: ECC disabled, Data cache writeback

[    0.000000] MX6_MAP_IO START

[    0.000000] CPU identified as i.MX6DL/SOLO, silicon rev 1.1

[    0.000000] MX6_MAP_IO END

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

[    0.000000] Kernel command line: console=ttymxc0,115200n8 rdinit=/linuxrc enable_wait_mode=off

[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)

[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

[    0.000000] allocated 4194304 bytes of page_cgroup

[    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups

[    0.000000] Memory: 1024MB = 1024MB total

[    0.000000] Memory: 1027284k/1027284k available, 21292k reserved, 360448K highmem

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

[    0.000000]     DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

[    0.000000]     vmalloc : 0xea800000 - 0xf2000000   ( 120 MB)

[    0.000000]     lowmem  : 0xc0000000 - 0xea000000   ( 672 MB)

[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

[    0.000000]       .init : 0xc0008000 - 0xc004c000   ( 272 kB)

[    0.000000]       .text : 0xc004c000 - 0xc0734000   (7072 kB)

[    0.000000]       .data : 0xc0734000 - 0xc0775a30   ( 263 kB)

[    0.000000]        .bss : 0xc0775a54 - 0xc07f8330   ( 523 kB)

[    0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

[    0.000000] NR_IRQS:496 nr_irqs:496 496

[    0.000000] MX6_INIT_IRQ START

[    0.000000] MXC GPIO hardware

[    0.000000] MX6_INIT_IRQ END

[    0.000000] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

[    0.000000] Set periph_clk's parent to pll2_pfd_400M!

[    0.000000] MXC_Early serial console at MMIO 0x21f4000 (options '115200n8')

[    0.000000] bootconsole [ttymxc0] enabled

[    0.000000] RETOUR early_console_setup(UART5_BASE_ADDR, uart_clk)

[    0.000000] Console: colour dummy device 80x30

[    0.252063] Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

[    0.340362] pid_max: default: 32768 minimum: 301

[    0.345198] Security Framework initialized

[    0.349369] AppArmor: AppArmor initialized

[    0.353588] Mount-cache hash table entries: 512

[    0.358212] type: sysfs flags: 4194304 name: sysfs

[    0.363088] Unable to handle kernel paging request at virtual address f22f0040

[    0.370339] pgd = c0004000

[    0.373084] [f22f0040] *pgd=00000000

[    0.376688] Internal error: Oops: 805 [#1]

[    0.380798] Modules linked in:

[    0.383879] CPU: 0    Not tainted  (3.0.35MasterLight_1A+ #39)

[    0.389757] PC is at printascii+0x1c/0x4c

[    0.393787] LR is at early_write+0x3c/0x48

[    0.397902] pc : [<c00553fc>]    lr : [<c00554a4>]    psr: 20000153

[    0.397910] sp : c0735c50  ip : c005547c  fp : c0735c64

[    0.409428] r10: 00000001  r9 : 00400000  r8 : 0000cf39

[    0.414673] r7 : cc090140  r6 : cc0c3e24  r5 : c0735c82  r4 : c0735c6d

[    0.421222] r3 : f22f0000  r2 : f22f0000  r1 : 0000003c  r0 : 00000000

[    0.427775] Flags: nzCv  IRQs on  FIQs off  Mode SVC_32  ISA ARM  Segment kernel

[    0.435197] Control: 10c53c7d  Table: 10004059  DAC: 00000015

[    0.440963] Process swapper (pid: 0, stack limit = 0xc0734260)

[    0.446818] Stack: (0xc0735c50 to 0xc0736000)

[    0.451194] 5c40:                                     c0736028 e9ff0400 c0735e80 c0735c68

[    0.459405] 5c60: c0055520 c0055474 c0735e88 493e363c 5f544547 4b434f4c 53204445 54524154

[    0.467613] 5c80: 00000a20 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    0.475820] 5ca0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    0.484029] 5cc0: c00741c0 00000000 00000000 00000000 00000000 00000000 c0736098 c07442c0

[    0.492238] 5ce0: c0739c2c c077797b c0744e20 c0735d20 c0735cfc c00741c0 c008cbe4 00000000

[    0.500448] 5d00: 0000000f c0739c00 ffffffff c0735d0c c0735d0c c0735d4c c0735d24 c0079c30

[    0.508657] 5d20: c00f0e00 c0734000 c0739c00 00000000 00000000 0000003c c077797b e9ff4120

[    0.516867] 5d40: c00a541c c00aa70c c0735d78 c0735d58 c00aa70c c006ca1c c00a0504 00000000

[    0.525076] 5d60: c0743c20 c0797f40 c0747788 00000001 00000100 c0735d98 c0735d84 c00a0504

[    0.533286] 5d80: c00abe54 c0797f40 c0797dcc c0735dd8 c0735d9c c008be4c c00a04d8 00000057

[    0.541496] 5da0: 00000001 00015220 c0735da8 c0735da8 00000001 c0797dcc 00000001 00000100

[    0.549705] 5dc0: c00847b8 00000000 c0797dd0 c0084c18 c0735ddc c00847b8 c0083650 c0735e24

[    0.557914] 5de0: c0735dec c02d7764 c02d6e70 00000000 00000000 00000000 ffffffff 00000000

[    0.566123] 5e00: 00000000 c02d7b68 e9ff1800 00000000 c07db28c 00000000 c0735e70 c0735e28

[    0.574333] 5e20: c02d7b68 c012816c 00000000 e9fd1f08 00000000 e9fee600 e9ff0400 c0735e58

[    0.582542] 5e40: c0735e4c c02d6f74 c07db28c e9ff0400 c07db28c e9fee600 e9ff0400 c07da10c

[    0.590752] 5e60: c018e164 c0735e90 c0735e74 271aed3f e9ff0400 c0735eb8 c0735e94 c01480dc

[    0.598962] 5e80: c00554e4 c06bac2b ed0ecf39 c0737220 7339bc01 e9ff0400 c074d8ec c074d8ec

[    0.607172] 5ea0: c0592860 00000000 c074d91c c0735ed8 c0735ebc c018b8a4 c01480b0 c0735ec8

[    0.615381] 5ec0: c0578838 e9ff0400 e9fee600 c0735ef8 c0735edc c018e290 c018b88c e9fd0000

[    0.623591] 5ee0: 00000000 c06d97b0 c074d91c c0735f2c c0735efc c0134bd4 c018e19c c0735f1c

[    0.631801] 5f00: c0735f0c e9fd0000 c06d97b0 00400000 c074d91c 00000000 412fc09a 00000000

[    0.640010] 5f20: c0735f50 c0735f30 c014aa98 c0134b5c 00000000 c07dbae0 00000000 c073b284

[    0.648220] 5f40: 10004059 c0735f60 c0735f54 c014aafc c014aa30 c0735f80 c0735f64 c001c1e0

[    0.656430] 5f60: c014aae4 00000000 00000000 c0737234 0003eaf5 c0735fa4 c0735f84 c001a984

[    0.664639] 5f80: c001c188 00000000 c001a340 c0132f48 c0737208 00000000 c0735fd0 c0735fa8

[    0.672848] 5fa0: c001a5b8 c001a900 00000000 c0735fd0 c0735fbc c001dc48 c0736ff8 c002e944

[    0.681058] 5fc0: cc0028c0 c0735ff4 c0735fd4 c0008990 c001a528 c0008370 c002e944 10c53c7d

[    0.689268] 5fe0: c0736084 c002e940 00000000 c0735ff8 1000803c c00086e8 00000000 00000000

[    0.697469] Backtrace:

[    0.699959] [<c0055468>] (early_write+0x0/0x48) from [<c0055520>] (early_printk+0x4c/0x6c)

[    0.708250]  r5:e9ff0400 r4:c0736028

[    0.711886] [<c00554d4>] (early_printk+0x0/0x6c) from [<c01480dc>] (iget_locked+0x38/0x218)

[    0.720265]  r3:7339bc01 r2:c0737220 r1:ed0ecf39 r0:c06bac2b

[    0.725994]  r4:e9ff0400

[    0.728568] [<c01480a4>] (iget_locked+0x0/0x218) from [<c018b8a4>] (sysfs_get_inode+0x24/0x198)

[    0.737309] [<c018b880>] (sysfs_get_inode+0x0/0x198) from [<c018e290>] (sysfs_mount+0x100/0x1ac)

[    0.746122]  r5:e9fee600 r4:e9ff0400

[    0.749747] [<c018e190>] (sysfs_mount+0x0/0x1ac) from [<c0134bd4>] (mount_fs+0x84/0x1ac)

[    0.757862]  r7:c074d91c r6:c06d97b0 r5:00000000 r4:e9fd0000

[    0.763607] [<c0134b50>] (mount_fs+0x0/0x1ac) from [<c014aa98>] (vfs_kern_mount+0x74/0xb4)

[    0.771908] [<c014aa24>] (vfs_kern_mount+0x0/0xb4) from [<c014aafc>] (kern_mount_data+0x24/0x28)

[    0.780720]  r8:10004059 r7:c073b284 r6:00000000 r5:c07dbae0 r4:00000000

[    0.787517] [<c014aad8>] (kern_mount_data+0x0/0x28) from [<c001c1e0>] (sysfs_init+0x64/0xc0)

[    0.796003] [<c001c17c>] (sysfs_init+0x0/0xc0) from [<c001a984>] (mnt_init+0x90/0x1a0)

[    0.803945]  r6:0003eaf5 r5:c0737234 r4:00000000

[    0.808628] [<c001a8f4>] (mnt_init+0x0/0x1a0) from [<c001a5b8>] (vfs_caches_init+0x9c/0x12c)

[    0.817092]  r5:00000000 r4:c0737208

[    0.820715] [<c001a51c>] (vfs_caches_init+0x0/0x12c) from [<c0008990>] (start_kernel+0x2b4/0x338)

[    0.829615]  r6:cc0028c0 r5:c002e944 r4:c0736ff8

[    0.834292] [<c00086dc>] (start_kernel+0x0/0x338) from [<1000803c>] (0x1000803c)

[    0.841711]  r6:c002e940 r5:c0736084 r4:10c53c7d

[    0.846386] Code: e3130001 01a03001 11a03002 ea000006 (e5831040)

[    0.852554] ---[ end trace da227214a82491b7 ]---

[    0.857196] Kernel panic - not syncing: Attempted to kill the idle task!

[    0.863940] Backtrace:

[    0.866447] [<c004ff40>] (dump_backtrace+0x0/0x114) from [<c0572b2c>] (dump_stack+0x20/0x24)

[    0.874936]  r6:c0734000 r5:0000000b r4:c077745c

[    0.879624] [<c0572b0c>] (dump_stack+0x0/0x24) from [<c0572e64>] (panic+0x64/0x18c)

[    0.887341] [<c0572e00>] (panic+0x0/0x18c) from [<c00817d0>] (do_exit+0xb0/0x6b0)

[    0.894849]  r3:c0734000 r2:00000000 r1:00000000 r0:c06ae6c0

[    0.900599]  r7:c00553fe

[    0.903163] [<c0081720>] (do_exit+0x0/0x6b0) from [<c00503e4>] (die+0x29c/0x30c)

[    0.910601]  r7:c00553fe

[    0.913172] [<c0050148>] (die+0x0/0x30c) from [<c0572b94>] (__do_kernel_fault.part.2+0x64/0x84)

[    0.921929] [<c0572b30>] (__do_kernel_fault.part.2+0x0/0x84) from [<c0056494>] (do_bad_area+0x84/0x88)

[    0.931266]  r7:c074b864

[    0.933868] [<c0056410>] (do_bad_area+0x0/0x88) from [<c057bda8>] (do_translation_fault+0xa0/0xac)

[    0.942855]  r7:00000000 r6:00000805 r5:c0004000 r4:c0007c88

[    0.948637] [<c057bd08>] (do_translation_fault+0x0/0xac) from [<c004c164>] (do_DataAbort+0x44/0xa8)

[    0.957730]  r7:c0735c08 r6:f22f0040 r5:c073bb30 r4:00000805

[    0.963479] [<c004c120>] (do_DataAbort+0x0/0xa8) from [<c0579880>] (__dabt_svc+0x40/0x60)

[    0.971702] Exception stack(0xc0735c08 to 0xc0735c50)

[    0.976777] 5c00:                   00000000 0000003c f22f0000 f22f0000 c0735c6d c0735c82

[    0.985006] 5c20: cc0c3e24 cc090140 0000cf39 00400000 00000001 c0735c64 c005547c c0735c50

[    0.993213] 5c40: c00554a4 c00553fc 20000153 ffffffff

[    0.998298]  r7:cc090140 r6:cc0c3e24 r5:c0735c3c r4:ffffffff

[    1.004051] [<c0055468>] (early_write+0x0/0x48) from [<c0055520>] (early_printk+0x4c/0x6c)

[    1.012362]  r5:e9ff0400 r4:c0736028

[    1.015998] [<c00554d4>] (early_printk+0x0/0x6c) from [<c01480dc>] (iget_locked+0x38/0x218)

[    1.024396]  r3:7339bc01 r2:c0737220 r1:ed0ecf39 r0:c06bac2b

[    1.030130]  r4:e9ff0400

[    1.032701] [<c01480a4>] (iget_locked+0x0/0x218) from [<c018b8a4>] (sysfs_get_inode+0x24/0x198)

[    1.041460] [<c018b880>] (sysfs_get_inode+0x0/0x198) from [<c018e290>] (sysfs_mount+0x100/0x1ac)

[    1.050275]  r5:e9fee600 r4:e9ff0400

[    1.053920] [<c018e190>] (sysfs_mount+0x0/0x1ac) from [<c0134bd4>] (mount_fs+0x84/0x1ac)

[    1.062038]  r7:c074d91c r6:c06d97b0 r5:00000000 r4:e9fd0000

[    1.067805] [<c0134b50>] (mount_fs+0x0/0x1ac) from [<c014aa98>] (vfs_kern_mount+0x74/0xb4)

[    1.076126] [<c014aa24>] (vfs_kern_mount+0x0/0xb4) from [<c014aafc>] (kern_mount_data+0x24/0x28)

[    1.084940]  r8:10004059 r7:c073b284 r6:00000000 r5:c07dbae0 r4:00000000

[    1.091760] [<c014aad8>] (kern_mount_data+0x0/0x28) from [<c001c1e0>] (sysfs_init+0x64/0xc0)

[    1.100263] [<c001c17c>] (sysfs_init+0x0/0xc0) from [<c001a984>] (mnt_init+0x90/0x1a0)

[    1.108206]  r6:0003eaf5 r5:c0737234 r4:00000000

[    1.112907] [<c001a8f4>] (mnt_init+0x0/0x1a0) from [<c001a5b8>] (vfs_caches_init+0x9c/0x12c)

[    1.121389]  r5:00000000 r4:c0737208

[    1.125018] [<c001a51c>] (vfs_caches_init+0x0/0x12c) from [<c0008990>] (start_kernel+0x2b4/0x338)

[    1.133936]  r6:cc0028c0 r5:c002e944 r4:c0736ff8

[    1.138618] [<c00086dc>] (start_kernel+0x0/0x338) from [<1000803c>] (0x1000803c)

[    1.146057]  r6:c002e940 r5:c0736084 r4:10c53c7d

Do you have any tips ? Where do i have to search the problem ?

Thanks.

Regards,

0 Kudos
Reply

2,725 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

What modification did you perform?

That might give us a clue of the possible problem.

Best Regards,

Alejandro

0 Kudos
Reply